<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 Inconsistent ADC Temperature Coefficients between SDK2.8.2 and UM11126</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Inconsistent-ADC-Temperature-Coefficients-between-SDK2/m-p/1159275#M42396</link>
    <description>&lt;P&gt;Hallo Everyone!&lt;/P&gt;&lt;P&gt;Just an observation on inconsistent ADC Temperature coefficient values between UM11126 vs values used by Configtool/SDK 2.8.2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I create a New C/C++ project from scratch in MCUXpresso using SDK2.8.2 for the LPC55s69 and add the lpadc driver, it adds the files fsl_lpadc.c and .h to the project, which also includes the&amp;nbsp;the function:&lt;/P&gt;&lt;P&gt;float LPADC_MeasureTemperature(ADC_Type *base, uint32_t commandId, uint32_t index)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the MeasureTemperature function it uses&amp;nbsp;FSL_FEATURE_LPADC_TEMP_PARAMETER_A,&amp;nbsp;FSL_FEATURE_LPADC_TEMP_PARAMETER_B &amp;amp;&amp;nbsp; FSL_FEATURE_LPADC_TEMP_PARAMETER_ALPHA, values defined in&amp;nbsp;LPC55S69_cm33_core0_FEATURES.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The values defined in UM11126 (39.7.6 p769) differs from the values used in&amp;nbsp;LPC55S69_cm33_core0_FEATURES.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which ones are correct for HW rev 1B?&lt;/P&gt;&lt;P&gt;Alpha : 8.5 vs 11.5&lt;/P&gt;&lt;P&gt;A : 804 vs 744.6&lt;/P&gt;&lt;P&gt;B : 280 vs 313.7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gert&lt;/P&gt;</description>
    <pubDate>Fri, 25 Sep 2020 10:21:03 GMT</pubDate>
    <dc:creator>gertvb</dc:creator>
    <dc:date>2020-09-25T10:21:03Z</dc:date>
    <item>
      <title>LPC55S69 Inconsistent ADC Temperature Coefficients between SDK2.8.2 and UM11126</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Inconsistent-ADC-Temperature-Coefficients-between-SDK2/m-p/1159275#M42396</link>
      <description>&lt;P&gt;Hallo Everyone!&lt;/P&gt;&lt;P&gt;Just an observation on inconsistent ADC Temperature coefficient values between UM11126 vs values used by Configtool/SDK 2.8.2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I create a New C/C++ project from scratch in MCUXpresso using SDK2.8.2 for the LPC55s69 and add the lpadc driver, it adds the files fsl_lpadc.c and .h to the project, which also includes the&amp;nbsp;the function:&lt;/P&gt;&lt;P&gt;float LPADC_MeasureTemperature(ADC_Type *base, uint32_t commandId, uint32_t index)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the MeasureTemperature function it uses&amp;nbsp;FSL_FEATURE_LPADC_TEMP_PARAMETER_A,&amp;nbsp;FSL_FEATURE_LPADC_TEMP_PARAMETER_B &amp;amp;&amp;nbsp; FSL_FEATURE_LPADC_TEMP_PARAMETER_ALPHA, values defined in&amp;nbsp;LPC55S69_cm33_core0_FEATURES.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The values defined in UM11126 (39.7.6 p769) differs from the values used in&amp;nbsp;LPC55S69_cm33_core0_FEATURES.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which ones are correct for HW rev 1B?&lt;/P&gt;&lt;P&gt;Alpha : 8.5 vs 11.5&lt;/P&gt;&lt;P&gt;A : 804 vs 744.6&lt;/P&gt;&lt;P&gt;B : 280 vs 313.7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gert&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 10:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Inconsistent-ADC-Temperature-Coefficients-between-SDK2/m-p/1159275#M42396</guid>
      <dc:creator>gertvb</dc:creator>
      <dc:date>2020-09-25T10:21:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 Inconsistent ADC Temperature Coefficients between SDK2.8.2 and UM11126</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Inconsistent-ADC-Temperature-Coefficients-between-SDK2/m-p/1160851#M42429</link>
      <description>&lt;P&gt;Hello &lt;A id="link_12" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154497" target="_self"&gt;gertvb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you use the values from the SDK.&lt;/P&gt;
&lt;P&gt;A = 744.6&lt;/P&gt;
&lt;P&gt;B = 313.7&lt;/P&gt;
&lt;P&gt;Alpha = 11.5&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for letting us know about the difference between the parameters.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 17:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Inconsistent-ADC-Temperature-Coefficients-between-SDK2/m-p/1160851#M42429</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-09-29T17:25:36Z</dc:date>
    </item>
  </channel>
</rss>