<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC802 output pin issue when initialize Uart</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-output-pin-issue-when-initialize-Uart/m-p/1158447#M42365</link>
    <description>&lt;P&gt;I've opened a new project and copy/paste my source c file from old to new one. In the new project all goes right.&lt;/P&gt;&lt;P&gt;Both projects have same board.c, clock_config.c, preipherals.c, pin_mux.c and source c files. I dont know why in old project it does not work and in the new one it works fine.&lt;/P&gt;&lt;P&gt;It creates some insecurity in me. Any idea where is the problem ?&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2020 07:23:11 GMT</pubDate>
    <dc:creator>asier</dc:creator>
    <dc:date>2020-09-24T07:23:11Z</dc:date>
    <item>
      <title>LPC802 output pin issue when initialize Uart</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-output-pin-issue-when-initialize-Uart/m-p/1157709#M42351</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was developing a code and all went fine until I decide to use a Uart TX pin. I chosed PIO0_14 and generated code with MCUxpresso to create pin_mux.c and peripherals.c.&lt;/P&gt;&lt;P&gt;I use another pin (PIO0_1) as test output pin, so that when code startes running I can see a pulse of some milisecond on PIO0_1 output pin.&lt;/P&gt;&lt;P&gt;When I was not using Uart I saw this pulse on PIO0_1, but as soon as I do "USART_Init(USART0, &amp;amp;config, CLOCK_GetFreq(kCLOCK_MainClk));" to initialize Uart, my output pulse on PIO0_1 does not work again.&lt;/P&gt;&lt;P&gt;Any helping will be apreciated.&lt;/P&gt;&lt;P&gt;Asier.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 11:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-output-pin-issue-when-initialize-Uart/m-p/1157709#M42351</guid>
      <dc:creator>asier</dc:creator>
      <dc:date>2020-09-23T11:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 output pin issue when initialize Uart</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-output-pin-issue-when-initialize-Uart/m-p/1158447#M42365</link>
      <description>&lt;P&gt;I've opened a new project and copy/paste my source c file from old to new one. In the new project all goes right.&lt;/P&gt;&lt;P&gt;Both projects have same board.c, clock_config.c, preipherals.c, pin_mux.c and source c files. I dont know why in old project it does not work and in the new one it works fine.&lt;/P&gt;&lt;P&gt;It creates some insecurity in me. Any idea where is the problem ?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 07:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-output-pin-issue-when-initialize-Uart/m-p/1158447#M42365</guid>
      <dc:creator>asier</dc:creator>
      <dc:date>2020-09-24T07:23:11Z</dc:date>
    </item>
  </channel>
</rss>