<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC55s69 : USB1 as host ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1157859#M42354</link>
    <description>&lt;P&gt;Hello again&lt;/P&gt;&lt;P&gt;According to the user manual, both usb0 and usb1 can be usb host.&lt;/P&gt;&lt;P&gt;Usb0 works fine, but i'd like to try usb1 as host (the "HS" port near the debug port)&lt;/P&gt;&lt;P&gt;Is there an example project using USB1 as host ? They all seem to use USB 0 (?)&lt;/P&gt;&lt;P&gt;On the MCUXPresso LPC55s69 board&amp;nbsp; :&lt;/P&gt;&lt;P&gt;* From a hw point of view , is just switching the J6 jumper to HS enough (?) Are there limitation to use USB0/1 as host/device or can i use any roles on any ports ?&lt;/P&gt;&lt;P&gt;* From a sw point of view, what is the correct device driver to use USB1 as host ? IP3516HS ? KHCI ?&lt;/P&gt;&lt;P&gt;something else ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Tres&lt;/P&gt;</description>
    <pubDate>Wed, 23 Sep 2020 15:36:46 GMT</pubDate>
    <dc:creator>trescurieux</dc:creator>
    <dc:date>2020-09-23T15:36:46Z</dc:date>
    <item>
      <title>LPC55s69 : USB1 as host ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1157859#M42354</link>
      <description>&lt;P&gt;Hello again&lt;/P&gt;&lt;P&gt;According to the user manual, both usb0 and usb1 can be usb host.&lt;/P&gt;&lt;P&gt;Usb0 works fine, but i'd like to try usb1 as host (the "HS" port near the debug port)&lt;/P&gt;&lt;P&gt;Is there an example project using USB1 as host ? They all seem to use USB 0 (?)&lt;/P&gt;&lt;P&gt;On the MCUXPresso LPC55s69 board&amp;nbsp; :&lt;/P&gt;&lt;P&gt;* From a hw point of view , is just switching the J6 jumper to HS enough (?) Are there limitation to use USB0/1 as host/device or can i use any roles on any ports ?&lt;/P&gt;&lt;P&gt;* From a sw point of view, what is the correct device driver to use USB1 as host ? IP3516HS ? KHCI ?&lt;/P&gt;&lt;P&gt;something else ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Tres&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 15:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1157859#M42354</guid>
      <dc:creator>trescurieux</dc:creator>
      <dc:date>2020-09-23T15:36:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55s69 : USB1 as host ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1160251#M42412</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154477"&gt;@trescurieux&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Is there an example project using USB1 as host? They all seem to use USB 0 (?)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you change in the usb_host_config.h, the&amp;nbsp;USB_HOST_CONFIG_OHCI to 0 and&amp;nbsp;USB_HOST_CONFIG_IP3516HS to 1, you should be able to use the HS USB.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;From a hw point of view , is just switching the J6 jumper to HS enough (?) Are there limitations to use USB0/1 as host/device or can i use any roles on any ports?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There isn't a limitation about the rol but additional to the J6 you need to short J11 for USB1 or J12 for USB0 to enable the host power.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;From a sw point of view, what is the correct device driver to use USB1 as host? IP3516HS ? KHCI ?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I will suggest to use the IP3516HS.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2020 18:52:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1160251#M42412</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-09-28T18:52:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55s69 : USB1 as host ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1160405#M42417</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 05:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55s69-USB1-as-host/m-p/1160405#M42417</guid>
      <dc:creator>trescurieux</dc:creator>
      <dc:date>2020-09-29T05:15:04Z</dc:date>
    </item>
  </channel>
</rss>