<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックsmd crystal(quartz) for LPC1549</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/smd-crystal-quartz-for-LPC1549/m-p/1154274#M42258</link>
    <description>&lt;P&gt;Could I use &lt;SPAN class="more-expander-item"&gt;&lt;A href="https://www.murata.com/en/products/productdata/8801162133534/SPEC-CSTNE12M0GH5L000R0.pdf" target="_blank" rel="noopener"&gt;CSTNE12M0GH5L000R0&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;12 Mhz smd crystal (quartz) for&amp;nbsp; LPC1549 with&amp;nbsp; USB(CDC) and CAN interfaces application?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;This quartz&amp;nbsp; has frequency tolerance&amp;nbsp; 0.07% and frequency stability&amp;nbsp; 0.11%,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;the built-in capacitors in case of&amp;nbsp; the part&amp;nbsp; are 33 pF (Uoscin -= 1.08V, Uoscout =1.3V&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;Before I used&lt;FONT size="3"&gt; &lt;SPAN&gt;P&lt;/SPAN&gt;&lt;SPAN&gt;R&lt;/SPAN&gt;&lt;SPAN&gt;Q&lt;/SPAN&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;2&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;SPAN&gt;R&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;V&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;L&amp;nbsp;&lt;FONT size="3"&gt; smd&lt;/FONT&gt; &lt;/SPAN&gt;quartz with 10 pF built-in capacitors&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;(Uoscin -= 1.0V, Uoscout =1.5V) and&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN class="more-expander-item"&gt;frequency tolerance&amp;nbsp; 0.1% and frequency stability&amp;nbsp; 0.1%.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;But it is not available now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;NXP also recommends the quartz with the external capacitors&amp;nbsp; 7-10 pF. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;in R_10075 "&lt;SPAN&gt;Driving LPC1500 with EPSON Cryst&lt;/SPAN&gt;&lt;SPAN&gt;als"&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Sep 2020 17:14:48 GMT</pubDate>
    <dc:creator>iharihar</dc:creator>
    <dc:date>2020-09-16T17:14:48Z</dc:date>
    <item>
      <title>smd crystal(quartz) for LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/smd-crystal-quartz-for-LPC1549/m-p/1154274#M42258</link>
      <description>&lt;P&gt;Could I use &lt;SPAN class="more-expander-item"&gt;&lt;A href="https://www.murata.com/en/products/productdata/8801162133534/SPEC-CSTNE12M0GH5L000R0.pdf" target="_blank" rel="noopener"&gt;CSTNE12M0GH5L000R0&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;12 Mhz smd crystal (quartz) for&amp;nbsp; LPC1549 with&amp;nbsp; USB(CDC) and CAN interfaces application?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;This quartz&amp;nbsp; has frequency tolerance&amp;nbsp; 0.07% and frequency stability&amp;nbsp; 0.11%,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;the built-in capacitors in case of&amp;nbsp; the part&amp;nbsp; are 33 pF (Uoscin -= 1.08V, Uoscout =1.3V&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;Before I used&lt;FONT size="3"&gt; &lt;SPAN&gt;P&lt;/SPAN&gt;&lt;SPAN&gt;R&lt;/SPAN&gt;&lt;SPAN&gt;Q&lt;/SPAN&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;2&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;C&lt;/SPAN&gt;&lt;SPAN&gt;R&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;V&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;L&amp;nbsp;&lt;FONT size="3"&gt; smd&lt;/FONT&gt; &lt;/SPAN&gt;quartz with 10 pF built-in capacitors&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;(Uoscin -= 1.0V, Uoscout =1.5V) and&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN class="more-expander-item"&gt;frequency tolerance&amp;nbsp; 0.1% and frequency stability&amp;nbsp; 0.1%.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;But it is not available now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;NXP also recommends the quartz with the external capacitors&amp;nbsp; 7-10 pF. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="more-expander-item"&gt;in R_10075 "&lt;SPAN&gt;Driving LPC1500 with EPSON Cryst&lt;/SPAN&gt;&lt;SPAN&gt;als"&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 17:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/smd-crystal-quartz-for-LPC1549/m-p/1154274#M42258</guid>
      <dc:creator>iharihar</dc:creator>
      <dc:date>2020-09-16T17:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: smd crystal(quartz) for LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/smd-crystal-quartz-for-LPC1549/m-p/1155107#M42278</link>
      <description>&lt;P&gt;Hello iharihar,&lt;/P&gt;
&lt;P&gt;We do not have a list of other recommended crystals you may use other than the ones listed on the R_10075 document and those used in our boards. I would strongly recommend using a crystal that is similar in characteristics to those recommended, especially if you will be using USB and CAN.&lt;/P&gt;
&lt;P&gt;From what I would see on the CSTNE12M0GH5L000R0 datasheet, it has both a much higher load capacitance and frequency tolerance. This would affect the drive load and problems with the high-speed interfaces, so I would recommend looking for a crystal with similar properties as those on the list. You may look for the datasheet of the recommended crystal for comparison.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 00:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/smd-crystal-quartz-for-LPC1549/m-p/1155107#M42278</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-09-18T00:39:10Z</dc:date>
    </item>
  </channel>
</rss>