<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1837 Boot ROM mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-Boot-ROM-mode/m-p/1153301#M42235</link>
    <description>&lt;P&gt;Hi, Ethan,&lt;/P&gt;&lt;P&gt;The "MSC" means that the USB module of LPC1837 can be enumerated as a disk driver after it is plugged into PC so that you can drag the *.bin file to the disk driver, the *.bin file will be saved into on-chip flash. If you set the P2_9/P2_8/P1_2/P1_1 as low/high/low/high, if you enter ISP mode by setting P2_7 as low during/after Reset, can you see the disk driver after you insert the USB0?&lt;/P&gt;&lt;P&gt;Anyway, I suggest you download the latest Flash Magic tools from the link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://flash-magic.informer.com/download/#downloading" target="_blank"&gt;https://flash-magic.informer.com/download/#downloading&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The tools can detect the USB automatically, pls try to download application code via USB with the tools.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Sep 2020 07:40:22 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-09-15T07:40:22Z</dc:date>
    <item>
      <title>LPC1837 Boot ROM mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-Boot-ROM-mode/m-p/1151830#M42193</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I check LPC1837 datasheet page 63 about boot ROM have related description for Mass Storage Class&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ethanchen_0-1599787160897.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124880iBD2FA5D6714AAB88/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ethanchen_0-1599787160897.png" alt="ethanchen_0-1599787160897.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Setting Boot source bit pin to USB0 or USB1?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ethanchen_1-1599787389380.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124881i08F430DA60519330/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ethanchen_1-1599787389380.png" alt="ethanchen_1-1599787389380.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;How to perform MSC boot?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ethan Chen&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 01:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-Boot-ROM-mode/m-p/1151830#M42193</guid>
      <dc:creator>ethanchen</dc:creator>
      <dc:date>2020-09-11T01:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1837 Boot ROM mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-Boot-ROM-mode/m-p/1153301#M42235</link>
      <description>&lt;P&gt;Hi, Ethan,&lt;/P&gt;&lt;P&gt;The "MSC" means that the USB module of LPC1837 can be enumerated as a disk driver after it is plugged into PC so that you can drag the *.bin file to the disk driver, the *.bin file will be saved into on-chip flash. If you set the P2_9/P2_8/P1_2/P1_1 as low/high/low/high, if you enter ISP mode by setting P2_7 as low during/after Reset, can you see the disk driver after you insert the USB0?&lt;/P&gt;&lt;P&gt;Anyway, I suggest you download the latest Flash Magic tools from the link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://flash-magic.informer.com/download/#downloading" target="_blank"&gt;https://flash-magic.informer.com/download/#downloading&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The tools can detect the USB automatically, pls try to download application code via USB with the tools.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Sep 2020 07:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1837-Boot-ROM-mode/m-p/1153301#M42235</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-09-15T07:40:22Z</dc:date>
    </item>
  </channel>
</rss>