<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1765 flash retention time</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-flash-retention-time/m-p/1134373#M42130</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to estimate the flash retention time for an LPC1765 constantly powered under a temperature of 40°C.&lt;/P&gt;&lt;P&gt;In the Reference Manual, the retention time for a powered device is 10 years min and 20years min for an unpowered device, but I look for a more precise estimation for a running without interruption at 40°C.&lt;/P&gt;&lt;P&gt;Support is much appreciated&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 02 Sep 2020 15:03:09 GMT</pubDate>
    <dc:creator>davidouatt08</dc:creator>
    <dc:date>2020-09-02T15:03:09Z</dc:date>
    <item>
      <title>LPC1765 flash retention time</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-flash-retention-time/m-p/1134373#M42130</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to estimate the flash retention time for an LPC1765 constantly powered under a temperature of 40°C.&lt;/P&gt;&lt;P&gt;In the Reference Manual, the retention time for a powered device is 10 years min and 20years min for an unpowered device, but I look for a more precise estimation for a running without interruption at 40°C.&lt;/P&gt;&lt;P&gt;Support is much appreciated&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 15:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-flash-retention-time/m-p/1134373#M42130</guid>
      <dc:creator>davidouatt08</dc:creator>
      <dc:date>2020-09-02T15:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1765 flash retention time</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-flash-retention-time/m-p/1138064#M42141</link>
      <description>&lt;P&gt;If the devices are using under all the specifications. those can support the 10 years at 40C, as you can see on the datasheet, this spec is from&amp;nbsp;Tamb = −40 °C to +85 °C.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You need to be sure while you are running at 40C continuously all the other specs are under spec, also the power consumption, read and write on memories, etc.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this will help you&lt;/P&gt;
&lt;P&gt;Have a good day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 17:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-flash-retention-time/m-p/1138064#M42141</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-09-03T17:50:34Z</dc:date>
    </item>
  </channel>
</rss>