<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC546xx IAP documentation error (UM10912)?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-IAP-documentation-error-UM10912/m-p/1096977#M42035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the UM10912, Chapter 5: LPC546xx ISP and IAP, Table 77.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;IAP Read Boot code version number&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Command:&amp;nbsp;&amp;nbsp;&amp;nbsp;Read boot code version number&lt;/P&gt;&lt;P&gt;Input:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Command code: 55 (decimal)&lt;/P&gt;&lt;P&gt;Result:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Result0: Two 32-bit words. Word 0 is the major version, word 1 is the minor version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when executing this command the result is &lt;STRONG&gt;NOT&lt;/STRONG&gt; two 32-bit words but two 8-bit bytes packed int Result0.&lt;/P&gt;&lt;P&gt;After executing the command the result in Result0 is 0x00001301 which means Major version 0x13 and Minor version 0x01.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2020 06:53:50 GMT</pubDate>
    <dc:creator>bwinter</dc:creator>
    <dc:date>2020-04-15T06:53:50Z</dc:date>
    <item>
      <title>LPC546xx IAP documentation error (UM10912)?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-IAP-documentation-error-UM10912/m-p/1096977#M42035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the UM10912, Chapter 5: LPC546xx ISP and IAP, Table 77.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;IAP Read Boot code version number&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Command:&amp;nbsp;&amp;nbsp;&amp;nbsp;Read boot code version number&lt;/P&gt;&lt;P&gt;Input:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Command code: 55 (decimal)&lt;/P&gt;&lt;P&gt;Result:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Result0: Two 32-bit words. Word 0 is the major version, word 1 is the minor version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when executing this command the result is &lt;STRONG&gt;NOT&lt;/STRONG&gt; two 32-bit words but two 8-bit bytes packed int Result0.&lt;/P&gt;&lt;P&gt;After executing the command the result in Result0 is 0x00001301 which means Major version 0x13 and Minor version 0x01.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 06:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-IAP-documentation-error-UM10912/m-p/1096977#M42035</guid>
      <dc:creator>bwinter</dc:creator>
      <dc:date>2020-04-15T06:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx IAP documentation error (UM10912)?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-IAP-documentation-error-UM10912/m-p/1096978#M42036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The lower 2 bytes with major/minor version number is the correct output format.&lt;/P&gt;&lt;P&gt;The user manual is wrong, as a consequence this could also be wrong in some tools like the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 08:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-IAP-documentation-error-UM10912/m-p/1096978#M42036</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-04-15T08:45:23Z</dc:date>
    </item>
  </channel>
</rss>