<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Programming using Python in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1096222#M42005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to write code for NXP controllers using python scripting?&lt;/P&gt;&lt;P&gt;Present using devices: LPC17xx, LPC546xx, LPC1519, MKE04 series, LPC8XX series.&lt;/P&gt;&lt;P&gt;If any of the device supports python, please suggest the IDE. Present using IDE: Keil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2020 07:50:26 GMT</pubDate>
    <dc:creator>TEMCEFF</dc:creator>
    <dc:date>2020-05-18T07:50:26Z</dc:date>
    <item>
      <title>Programming using Python</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1096222#M42005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to write code for NXP controllers using python scripting?&lt;/P&gt;&lt;P&gt;Present using devices: LPC17xx, LPC546xx, LPC1519, MKE04 series, LPC8XX series.&lt;/P&gt;&lt;P&gt;If any of the device supports python, please suggest the IDE. Present using IDE: Keil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 07:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1096222#M42005</guid>
      <dc:creator>TEMCEFF</dc:creator>
      <dc:date>2020-05-18T07:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: Programming using Python</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1096223#M42006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Very very unlikely, given the size of the python runtime vs the amount of Flash on Ram on ANY microcontroller. I have seen a thing called microPython which claims to fit in 256k of Flash and 16k of RAM, but I don't know if that is available on NXP devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 08:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1096223#M42006</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-05-18T08:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: Programming using Python</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1371387#M47006</link>
      <description>&lt;P&gt;MicroyPthon is available for some i.MX RT10xx controllers. See &lt;A href="https://micropython.org/download/?port=mimxrt" target="_blank"&gt;https://micropython.org/download/?port=mimxrt&lt;/A&gt; for binaries, and the MicroPyhton GitHub repository for the source code. The port is evolving, and its two other MicroPython users and me pushing it forward.&amp;nbsp; Until now, it is not tested on MIMXRT1060_EVK and MIMXRT1064_EVK boards, since these are on back-order at the common suppliers, with lead times of 6-12 months. So if someone is listening which has access to these board models, it would be helpful to test the firmware on these. Just upload them. If all works fine, there should be a REPL prompt at the USB port, and the internal flash should contain a lfs2 file system.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Nov 2021 14:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-using-Python/m-p/1371387#M47006</guid>
      <dc:creator>robert-hh</dc:creator>
      <dc:date>2021-11-15T14:36:54Z</dc:date>
    </item>
  </channel>
</rss>