<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC Link 2 destroys MCU when flashing in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094737#M41935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I will keep debugging.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My go to at the moment is not to use PoE and flash the MCU at the same time.&lt;/P&gt;&lt;P&gt;Since PoE and the LPC Link2 will not be connected at the same time during manufacturing, I am not that concerned about it anymore.&lt;BR /&gt;Still a weird behavior and worth looking into.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks for your suggestions!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 May 2020 20:37:28 GMT</pubDate>
    <dc:creator>jana_beck</dc:creator>
    <dc:date>2020-05-19T20:37:28Z</dc:date>
    <item>
      <title>LPC Link 2 destroys MCU when flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094733#M41931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I am having a very strange behavior.&lt;BR /&gt;When flashing my custom board, that has a LPC540 on it, the MCU gets destroyed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Setup:&lt;BR /&gt;&amp;nbsp;- The custom board is powered via PoE. That voltage is brought down to 3.3V.&amp;nbsp; I measured this voltage as well as ripple and it is all good.&lt;BR /&gt;- A LPC Link2 is connected via a 10 Pin JTAG header&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Test:&lt;BR /&gt;-2.1: No PoE and setting JP2 (and therefore powering the custom board from the LPC Link2) and flashing the MCU works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.2: PoE and not setting JP2. Everything is ok, until I flash the MCU. The board gets destroyed (I cannot talk to the MCU at all anymore and the PoE stops working as well (cycling on and off)&lt;BR /&gt;2.3: PoE, setting JP2, but separating the power (3.3V) coming from the LPC Link2 from the power (3.3V) on the custom board. Same behavior as 2.2.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2.3: PoE and setting JP2. Flashing works.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Can anyone tell me why this is happening and also why this is only happening when I try to flash?&lt;BR /&gt;When I set JP2, the LPC Link2 is already outputting 3.3V to my custom board, so why is this only happening once I flash?&lt;BR /&gt;&lt;BR /&gt;Any help appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 May 2020 01:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094733#M41931</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-17T01:02:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 destroys MCU when flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094734#M41932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With "destroyed", do you mean physically destroyed (casing blown, short circuit, high impedance), or just "no target detected" ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And with PoE, you mean power-over-ethernet ?&lt;/P&gt;&lt;P&gt;If yes, you might have a problem with your power supply, perhaps a GND potential issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 08:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094734#M41932</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2020-05-18T08:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 destroys MCU when flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094735#M41933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. The MCU does not work at all after flashing. Flashing destroys something on the board. After flashing, the 3.3 V power repeatedly turns on and off (which is I assume the PoE switch trying to output power, detects a failure and retries again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PoE= Power over Ethernet.&lt;BR /&gt;I need to double check thee GND potenial issue you are mentioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I still do not understand is, why this is happening only once I flash&amp;nbsp;the MCU.&lt;BR /&gt;Also, why is this not happening at all if I keep JP2 connected?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 16:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094735#M41933</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-18T16:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 destroys MCU when flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094736#M41934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would suggest to first check the power consumption.&lt;/P&gt;&lt;P&gt;I had not been working with NXP Cortex M devices for years, so I'm not an expert, to put it that way.&lt;/P&gt;&lt;P&gt;But your board might just be virtually bricked. Either the application is uncooperative (sleep modes often cause problems), or the Flashis corrupted, and the device starts into a ROM system bootloader.&lt;/P&gt;&lt;P&gt;I would try a mass erase, don't know what specific tools NXP offers in this case. But this was the way to go with other Cortex M devices I worked with (ST, Fujitsu/Cypress,&amp;nbsp;Atmel).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 10:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094736#M41934</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2020-05-19T10:27:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link 2 destroys MCU when flashing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094737#M41935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I will keep debugging.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My go to at the moment is not to use PoE and flash the MCU at the same time.&lt;/P&gt;&lt;P&gt;Since PoE and the LPC Link2 will not be connected at the same time during manufacturing, I am not that concerned about it anymore.&lt;BR /&gt;Still a weird behavior and worth looking into.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks for your suggestions!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 20:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-Link-2-destroys-MCU-when-flashing/m-p/1094737#M41935</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-19T20:37:28Z</dc:date>
    </item>
  </channel>
</rss>