<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1765 Startup time?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-Startup-time/m-p/1094251#M41925</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Florian,&lt;/P&gt;&lt;P&gt;Pls refer to the following table, copied from UM10360.pdf.&lt;/P&gt;&lt;P&gt;It describes the time from rising Rest signal to the instant that the user code is executed.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115717i65C0D3A62E271C2C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2020 05:48:37 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-07-14T05:48:37Z</dc:date>
    <item>
      <title>LPC1765 Startup time?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-Startup-time/m-p/1094250#M41924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question regarding the startup time of the LPC1765 CPU: How long does it take for the Chip to start up and start executing the user program? Or in other words: Assuming that a stable power source is attached, how long does it take until the chip executes the first user instruction after the power source is attached? I couldn't find anything in the datasheet about that, just that the flash wake-up timer generates a 100uS startup time and then 250 additional clock cycles are needed. As the user program is stored in the flash, the startup time is higher than 100uS + 250 clock cycles I assume?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 18:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-Startup-time/m-p/1094250#M41924</guid>
      <dc:creator>flole</dc:creator>
      <dc:date>2020-07-13T18:29:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1765 Startup time?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-Startup-time/m-p/1094251#M41925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Florian,&lt;/P&gt;&lt;P&gt;Pls refer to the following table, copied from UM10360.pdf.&lt;/P&gt;&lt;P&gt;It describes the time from rising Rest signal to the instant that the user code is executed.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115717i65C0D3A62E271C2C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 05:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-Startup-time/m-p/1094251#M41925</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-07-14T05:48:37Z</dc:date>
    </item>
  </channel>
</rss>