<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I am going to attempt to make a computerized chess board that uses NFC tags in the pieces and readers in the board to locate the pieces. My problem is that I cannot find NFC readers small enough to put into the squares if the chess board. Can anyone s in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-am-going-to-attempt-to-make-a-computerized-chess-board-that/m-p/1092960#M41873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the size requirement? We have PN736x family which offers an all in one solution, with features such as NFC, microcontroller, and software in a single chip. please kindly refer to&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf" title="https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2020 07:42:05 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-07-15T07:42:05Z</dc:date>
    <item>
      <title>I am going to attempt to make a computerized chess board that uses NFC tags in the pieces and readers in the board to locate the pieces. My problem is that I cannot find NFC readers small enough to put into the squares if the chess board. Can anyone sugge</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-am-going-to-attempt-to-make-a-computerized-chess-board-that/m-p/1092959#M41872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I wanted to put individual readers into the squares on the chess board but I cannot find any simple, small NFC readers that I can use in this situation. I also want to plug them into a pi for the computations, but I am open to other suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2020 04:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-am-going-to-attempt-to-make-a-computerized-chess-board-that/m-p/1092959#M41872</guid>
      <dc:creator>carlucci987</dc:creator>
      <dc:date>2020-07-13T04:46:01Z</dc:date>
    </item>
    <item>
      <title>Re: I am going to attempt to make a computerized chess board that uses NFC tags in the pieces and readers in the board to locate the pieces. My problem is that I cannot find NFC readers small enough to put into the squares if the chess board. Can anyone s</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-am-going-to-attempt-to-make-a-computerized-chess-board-that/m-p/1092960#M41873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the size requirement? We have PN736x family which offers an all in one solution, with features such as NFC, microcontroller, and software in a single chip. please kindly refer to&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf" title="https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/PN736XDS.pdf&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 07:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-am-going-to-attempt-to-make-a-computerized-chess-board-that/m-p/1092960#M41873</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-07-15T07:42:05Z</dc:date>
    </item>
  </channel>
</rss>