<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックTerminate, build and debug</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Terminate-build-and-debug/m-p/1083052#M41609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've recently upgraded to 11.1.1, and I note that the function called "terminate, build and debug" now only does "terminate and debug" even though it is still labelled "terminate, build and debug". I didn't see any information on this in the list of changes. How can I get it back to doing all three?&lt;/P&gt;&lt;P&gt;Also, I note that even when "debug" is selected it occasionally does "attach" instead. The only way I have found to reset it, is to select "erase flash via linkserver", erase the flash, then reselect "debug" and which point I get the dialogue box asking if I really want "debug" not "attach", and after that it works. Is there a better way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2020 13:53:21 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2020-08-11T13:53:21Z</dc:date>
    <item>
      <title>Terminate, build and debug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Terminate-build-and-debug/m-p/1083052#M41609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've recently upgraded to 11.1.1, and I note that the function called "terminate, build and debug" now only does "terminate and debug" even though it is still labelled "terminate, build and debug". I didn't see any information on this in the list of changes. How can I get it back to doing all three?&lt;/P&gt;&lt;P&gt;Also, I note that even when "debug" is selected it occasionally does "attach" instead. The only way I have found to reset it, is to select "erase flash via linkserver", erase the flash, then reselect "debug" and which point I get the dialogue box asking if I really want "debug" not "attach", and after that it works. Is there a better way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 13:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Terminate-build-and-debug/m-p/1083052#M41609</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2020-08-11T13:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: Terminate, build and debug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Terminate-build-and-debug/m-p/1083053#M41610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure whether you mean 'Build (if required before launching' with 'build':&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110077i757ACE33BB4AFEB6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Same about the second part ('attach'): The short solution would be to delete the launch configuration and then create a new one. Maybe untick 'attach' on the Debugger Tab of your launch configuration (depends on your debugger...).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 15:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Terminate-build-and-debug/m-p/1083053#M41610</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2020-08-11T15:08:04Z</dc:date>
    </item>
  </channel>
</rss>