<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC546xx USB_VBUS</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082354#M41601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had been looking at the datasheet revision 2.6, and it seems this table was added back in Feburary 2020 to revision 2.7; not noticing that was perhaps an oversight on my behalf. In addition to this table it would very useful if the 'Function' listed in the table could be described. I have searched the document and can find no explaination of 'VBUS_valid'. I might guess but I would prefer to have the NXP explain the term as it is intended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, and perhaps it is even more important that I note the revision of the datasheet has also changed the title of section 13.7 from "&lt;SPAN style="text-decoration: underline;"&gt;Suggested USB interface solutions&lt;/SPAN&gt;" to &lt;SPAN style="text-decoration: underline; color: #000000;"&gt;"Suggested &lt;STRONG&gt;USB0&lt;/STRONG&gt; Full-speed interface solutions&lt;/SPAN&gt;". And the table you show above is in a new section "13.8 USB1 High-speed VBUS threshold levels".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, is it the case that the voltages for USB1 (and given in Table 59) are now different from those previously specified in the datasheet for both USB interfaces?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These new figures do not seem to correspond in any way with the previous description, and I would consider this a very significant alteration of the specification!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Padraig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jun 2020 08:55:03 GMT</pubDate>
    <dc:creator>padraig_fogarty</dc:creator>
    <dc:date>2020-06-05T08:55:03Z</dc:date>
    <item>
      <title>LPC546xx USB_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082350#M41597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Figure 48 from the LPC546xx datasheet shows the pullup on USB_DP being switched from Vdd. However my understanding is that the USB specification requires this to be connected to USB_VBUS.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108230i1C61901E30D31107/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Given the problems I have seen with regard to USB device enumeration I suspect that the figure is in fact incorrect and the device does switch to USB_VBUS, but I would appreciate it if someone could confirm this detail. Also, if the minimum working voltage for the USB_VBUS could be provided that would also be very helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Padraig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 18:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082350#M41597</guid>
      <dc:creator>padraig_fogarty</dc:creator>
      <dc:date>2020-05-27T18:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082351#M41598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Padraig,&lt;/P&gt;&lt;P&gt;I have confirmed with AE team, the "Fig 48. USB interface on a self-powered device where USB_VBUS = 5 V" is correct, the USB_DP is pulled up to VDD instead of USB_VBUS with the DCON bit is set in the DEVCMDSTAT register.&lt;/P&gt;&lt;P&gt;Regarding the minimum voltage of the USB_VBUS pin, it is VDD*0.7, if the VDD is 3.3V, it is 0.7*3.3V=2.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 03:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082351#M41598</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-06-03T03:50:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082352#M41599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the response.&lt;/P&gt;&lt;P&gt;However, I find the details concerning since I my understanding is that the USB standard requires that USB_DP be pulled up to VBUS and not VDD; or at least that the pull-up should not be attached if VBUS is not present. Can you confirm how this works on the LPCxxx?&lt;/P&gt;&lt;P&gt;Also, from my own testing I can say that USB device enumeration will fail if the voltage on the USB_VBUS pin is below 2.9V. It certainly does not work anywhere close to 2.3V!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 11:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082352#M41599</guid>
      <dc:creator>padraig_fogarty</dc:creator>
      <dc:date>2020-06-03T11:54:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082353#M41600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Padraig,&lt;/P&gt;&lt;P&gt;This is the USB_VBUS pin voltage specs in data sheet of LPC546xx, pls refer to it.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112036iB6993247FB108281/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2020 03:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082353#M41600</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-06-05T03:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx USB_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082354#M41601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had been looking at the datasheet revision 2.6, and it seems this table was added back in Feburary 2020 to revision 2.7; not noticing that was perhaps an oversight on my behalf. In addition to this table it would very useful if the 'Function' listed in the table could be described. I have searched the document and can find no explaination of 'VBUS_valid'. I might guess but I would prefer to have the NXP explain the term as it is intended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, and perhaps it is even more important that I note the revision of the datasheet has also changed the title of section 13.7 from "&lt;SPAN style="text-decoration: underline;"&gt;Suggested USB interface solutions&lt;/SPAN&gt;" to &lt;SPAN style="text-decoration: underline; color: #000000;"&gt;"Suggested &lt;STRONG&gt;USB0&lt;/STRONG&gt; Full-speed interface solutions&lt;/SPAN&gt;". And the table you show above is in a new section "13.8 USB1 High-speed VBUS threshold levels".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, is it the case that the voltages for USB1 (and given in Table 59) are now different from those previously specified in the datasheet for both USB interfaces?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These new figures do not seem to correspond in any way with the previous description, and I would consider this a very significant alteration of the specification!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Padraig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2020 08:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-USB-VBUS/m-p/1082354#M41601</guid>
      <dc:creator>padraig_fogarty</dc:creator>
      <dc:date>2020-06-05T08:55:03Z</dc:date>
    </item>
  </channel>
</rss>