<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe:  LPC54018 EMC track length matching</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082327#M41596</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your patience,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="color: black;"&gt;Regarding chapter 5,&amp;nbsp; two inches is the limit for each branch stub. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Stub lengths are also included in the data bus length. The value for termination resistors depends on the impedance of the traces and since they are not required on all cases, the application note does not recommend an specific value. A calculation of their value needs to be performed.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;Typically, only high speed signals like&amp;nbsp; DATA&amp;nbsp; require a termination resistors.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Additionally, &amp;nbsp;&amp;nbsp;you could take into account the following advice made by one of our colleagues on the post:&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/message/1021648?commentID=1021648#comment-1021648"&gt;&lt;SPAN style="color: blue;"&gt;Impedance Control EMC Signals LPC4370 &lt;/SPAN&gt;&lt;/A&gt;. The frequency of the SDRAM data signals could be taken into account , for example a SRAM with 120 MHz could not be consider as&amp;nbsp; high speed, however proper impedance match have to be done to avoid issues. &lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Regards,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2020 02:01:59 GMT</pubDate>
    <dc:creator>diego_charles</dc:creator>
    <dc:date>2020-06-26T02:01:59Z</dc:date>
    <item>
      <title>LPC54018 EMC track length matching</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082323#M41592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using LPC54018 with external parallel NOR flash and SDRAM. The address bus is different lengths for both does the track lengths need to be matched to a particular accuracy. Also the JTAG and BOOT share pins with the bus is there any guidelines for managing connection of these to the data bus?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 10:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082323#M41592</guid>
      <dc:creator>adrian_lavin</dc:creator>
      <dc:date>2020-06-10T10:43:38Z</dc:date>
    </item>
    <item>
      <title>Re:  LPC54018 EMC track length matching</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082324#M41593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the delay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P lang="es-MX"&gt;At this moment you may have found the &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf#page=1&amp;amp;zoom=auto,-144,799"&gt;AN12026 SDRAM interface to LPC546xx external memory controller&lt;/A&gt;&lt;/P&gt;&lt;P lang="es-MX"&gt;However , I am able to point out the&amp;nbsp; chapter&amp;nbsp; 5&amp;nbsp; Schematics, PCB design tips and suggestions, that provides guidelines for trace lenghts , trace impedance and compensation for clock fligth time.&lt;/P&gt;&lt;P lang="es-MX"&gt;&lt;/P&gt;&lt;P lang="es-MX"&gt;If I can help further, please do not hesitate to reply.&lt;/P&gt;&lt;P lang="es-MX"&gt;Regards,&lt;/P&gt;&lt;P lang="es-MX"&gt;Diego&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 04:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082324#M41593</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2020-06-17T04:35:59Z</dc:date>
    </item>
    <item>
      <title>Re:  LPC54018 EMC track length matching</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082325#M41594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;Thanks for the replay, yes I have reviewed chapter 5 and would the following be correct:&lt;/P&gt;&lt;P&gt;For our design we have one SDRAM, one NOR Flash (shares A0-A14, D0 to D15 and WEN with SDRAM), JTAG (shares D0 to D4 with SDRAM) and Boot pins (share D2 to D4 with SDRAM).&lt;/P&gt;&lt;P&gt;Layout will be MCU at one end the SDRAM at the other end and the Flash, Jtag, Boot in between the two devices.&lt;/P&gt;&lt;P&gt;The introduction to chapter 5 mentions branch stubs of no more than 2inches, does this refer to the track shown in orange below, is this the limit for the length on each stub or total?&lt;/P&gt;&lt;P&gt;CLK0 routed from the MCU to the SDRAM directly with trace impedance of 60-80ohms. Length is not critical as it can be tuned with internal delays.&lt;/P&gt;&lt;P&gt;All other signals routed with impedance of 80-100ohms&lt;/P&gt;&lt;P&gt;In section 5.3, if the data bus is longer than 1.5inches total (does this include the stub lengths?) use series termination resistors, is there a recommended value? Is this only for the data bus signals to any other signal have to comply with this requirement?&lt;/P&gt;&lt;P&gt;Section 5.4.1, Rule 1, does the 2 inches of length matching refer to the trace length directly from the MCU to the SDRAM (just the red trace below) or does it also include the stub lengths as well? For example can EMC_D0 from MCU to SDRAM be two inches longer or shorter than EMC_CAS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SULZER CONFIDENTIAL&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 12:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082325#M41594</guid>
      <dc:creator>adrian_lavin</dc:creator>
      <dc:date>2020-06-17T12:58:45Z</dc:date>
    </item>
    <item>
      <title>Re:  LPC54018 EMC track length matching</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082326#M41595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply, please provide me additional time to provide you my feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 03:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082326#M41595</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2020-06-19T03:01:01Z</dc:date>
    </item>
    <item>
      <title>Re:  LPC54018 EMC track length matching</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082327#M41596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your patience,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="color: black;"&gt;Regarding chapter 5,&amp;nbsp; two inches is the limit for each branch stub. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Stub lengths are also included in the data bus length. The value for termination resistors depends on the impedance of the traces and since they are not required on all cases, the application note does not recommend an specific value. A calculation of their value needs to be performed.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;Typically, only high speed signals like&amp;nbsp; DATA&amp;nbsp; require a termination resistors.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Additionally, &amp;nbsp;&amp;nbsp;you could take into account the following advice made by one of our colleagues on the post:&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/message/1021648?commentID=1021648#comment-1021648"&gt;&lt;SPAN style="color: blue;"&gt;Impedance Control EMC Signals LPC4370 &lt;/SPAN&gt;&lt;/A&gt;. The frequency of the SDRAM data signals could be taken into account , for example a SRAM with 120 MHz could not be consider as&amp;nbsp; high speed, however proper impedance match have to be done to avoid issues. &lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Regards,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2020 02:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-EMC-track-length-matching/m-p/1082327#M41596</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2020-06-26T02:01:59Z</dc:date>
    </item>
  </channel>
</rss>