<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic connect LPC 4370 (link-2) using USB to ethernet adapter in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081346#M41539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on a project dealing with transferring ADC data to PC, However the provided peripherals do not have the speed needed for transferring ADC data which in my case is 60MHz do you guys have any suggestion? if unfortunately there is no way i decided to transfer data through usb to ethernet adapter which is more industrial than USB but the point is the ethernet program does not recognize it and gives the error "the device actively refuses connection" i would very much appreciate any help. thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2020 08:56:02 GMT</pubDate>
    <dc:creator>navidfanaee</dc:creator>
    <dc:date>2020-07-09T08:56:02Z</dc:date>
    <item>
      <title>connect LPC 4370 (link-2) using USB to ethernet adapter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081346#M41539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on a project dealing with transferring ADC data to PC, However the provided peripherals do not have the speed needed for transferring ADC data which in my case is 60MHz do you guys have any suggestion? if unfortunately there is no way i decided to transfer data through usb to ethernet adapter which is more industrial than USB but the point is the ethernet program does not recognize it and gives the error "the device actively refuses connection" i would very much appreciate any help. thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2020 08:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081346#M41539</guid>
      <dc:creator>navidfanaee</dc:creator>
      <dc:date>2020-07-09T08:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: connect LPC 4370 (link-2) using USB to ethernet adapter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081347#M41540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Hi Navid, I hope you're doing well!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to the&lt;A href="https://www.nxp.com/docs/en/data-sheet/LPC4370.pdf"&gt; LPC4370's Datasheet&lt;/A&gt;, Ethernet's Dynamic Characteristics are as follows, with speeds of 10/100 Mbit/s:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115823i1FE71D17EC488EF7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, there's no example code designed for an USB to Ethernet Converter included in the LPC4370's LPC-Open code bundle, but there's extensive documentation regarding the USB Stack as well as some example projects included in the &lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc43xx:LPCOPEN-SOFTWARE-FOR-LPC43XX"&gt;LPC-Open package&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if you need any more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 20:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081347#M41540</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-07-14T20:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: connect LPC 4370 (link-2) using USB to ethernet adapter</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081348#M41541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your time and response. sadly I couldn't find a way to transmit data with the desired rate and i also couldn't use usb to ethernet adapter as it seems that it doesnt recognize the ARM USB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 15:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/connect-LPC-4370-link-2-using-USB-to-ethernet-adapter/m-p/1081348#M41541</guid>
      <dc:creator>navidfanaee</dc:creator>
      <dc:date>2020-07-15T15:20:53Z</dc:date>
    </item>
  </channel>
</rss>