<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: How can I disable secure boot on LPC55S69 after I've enabled it?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-disable-secure-boot-on-LPC55S69-after-I-ve-enabled-it/m-p/1078489#M41490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Conor,&lt;/P&gt;&lt;P&gt;Once secure boot is enabled by setting CMPA, there is no way to disable it. Enabling secure boot is the last step of developing， it's&amp;nbsp;irreversible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Apr 2020 10:22:08 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2020-04-27T10:22:08Z</dc:date>
    <item>
      <title>How can I disable secure boot on LPC55S69 after I've enabled it?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-disable-secure-boot-on-LPC55S69-after-I-ve-enabled-it/m-p/1078488#M41489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been closely following AN12283 and the chip reference manual.&amp;nbsp; I am trying to evaluate secure boot on my LPCXpresso55S69.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the mistake of enabling secure boot through the boot ROM before programming a signed image.&amp;nbsp; I used "elftosb-gui" in the 2.7.1 SDK to set secure boot to boot signed images, and then I reset the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can no longer program any flash from the boot rom, or I get "Command disallowed when security is enabled".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can still access the device and program flash using my JLINK debugger, but it is unable to execute any of the code.&amp;nbsp; I tried programming a signed application with the JLINK, but to no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see the CMPA page through JLINK/GDB, and I see SECURE_BOOT_CFG == 0x40000000, meaning secure boot is indeed enabled.&amp;nbsp; I have tried numerous times to set SECURE_BOOT_CFG back to 0 using GDB, but none of my writes to CMPA work.&amp;nbsp; Seems CMPA is immutable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not seal any configuration with a sha256 hash, so I was under the impression I could roll back any changes but I haven't figured out how.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyway I can turn off secure boot and try again?&amp;nbsp; How?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Apr 2020 18:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-disable-secure-boot-on-LPC55S69-after-I-ve-enabled-it/m-p/1078488#M41489</guid>
      <dc:creator>cp1</dc:creator>
      <dc:date>2020-04-25T18:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: How can I disable secure boot on LPC55S69 after I've enabled it?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-disable-secure-boot-on-LPC55S69-after-I-ve-enabled-it/m-p/1078489#M41490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Conor,&lt;/P&gt;&lt;P&gt;Once secure boot is enabled by setting CMPA, there is no way to disable it. Enabling secure boot is the last step of developing， it's&amp;nbsp;irreversible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2020 10:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-can-I-disable-secure-boot-on-LPC55S69-after-I-ve-enabled-it/m-p/1078489#M41490</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-04-27T10:22:08Z</dc:date>
    </item>
  </channel>
</rss>