<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC SIGTRAP error &amp;quot;Break at address with no debug information...&amp;quot;</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076419#M41447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Swetha,&lt;/P&gt;&lt;P&gt;Thank you for contacting us.&lt;/P&gt;&lt;P&gt;First we need to identify the problem is on project or IDE system.&lt;/P&gt;&lt;P&gt;Please create a NEW workspace and import a NEW demo code ( for example led blink demo), see if the problem exists? if no issue, import your working project into this new workspace, how is the connecting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 06:35:20 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2020-06-10T06:35:20Z</dc:date>
    <item>
      <title>LPC SIGTRAP error "Break at address with no debug information..."</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076418#M41446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After changing the I/O in an example project running on a board that uses the LPC55S66JBD100 and starting the debug session, the following SIGTRAP error occurs. What could cause this error? Issue with the code or the debugger configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112410iC15661A099AF59E7/image-size/large?v=v2&amp;amp;px=999" title="error_log.PNG" alt="error_log.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 00:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076418#M41446</guid>
      <dc:creator>swetha_v</dc:creator>
      <dc:date>2020-06-10T00:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC SIGTRAP error "Break at address with no debug information..."</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076419#M41447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Swetha,&lt;/P&gt;&lt;P&gt;Thank you for contacting us.&lt;/P&gt;&lt;P&gt;First we need to identify the problem is on project or IDE system.&lt;/P&gt;&lt;P&gt;Please create a NEW workspace and import a NEW demo code ( for example led blink demo), see if the problem exists? if no issue, import your working project into this new workspace, how is the connecting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 06:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076419#M41447</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-06-10T06:35:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC SIGTRAP error "Break at address with no debug information..."</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076420#M41448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like it is possibly stack corruption. When you say "Changing the I/O" what do you actually mean - what, exactly, did you change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 08:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-SIGTRAP-error-quot-Break-at-address-with-no-debug/m-p/1076420#M41448</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-06-10T08:21:19Z</dc:date>
    </item>
  </channel>
</rss>