<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Is LPC54608 simulator available</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-LPC54608-simulator-available/m-p/1069668#M41256</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prathap,&lt;/P&gt;&lt;P&gt;As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Apr 2020 09:57:09 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-04-23T09:57:09Z</dc:date>
    <item>
      <title>Is LPC54608 simulator available</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-LPC54608-simulator-available/m-p/1069667#M41255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using mcuxpresso IDE for LPC54608 code development.&lt;/P&gt;&lt;P&gt;There is some issue to get my ordered kit delay(COVID issue).IS there any possible to debug and verify code level development without hardware setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;prathap&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 05:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-LPC54608-simulator-available/m-p/1069667#M41255</guid>
      <dc:creator>prathap_ponnuch</dc:creator>
      <dc:date>2020-04-23T05:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: Is LPC54608 simulator available</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-LPC54608-simulator-available/m-p/1069668#M41256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prathap,&lt;/P&gt;&lt;P&gt;As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 09:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-LPC54608-simulator-available/m-p/1069668#M41256</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-04-23T09:57:09Z</dc:date>
    </item>
  </channel>
</rss>