<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC55S69, DMA and DMA_ITRIG_INMUX</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067020#M41196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project where i need to read a GPIO port at a fixed frequency (a couple of MHz) and I want to use a DMA triggered by a CTIMER to achieve that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All of which seems totally possible according to reference manual (UM11126).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, when i read chapter 22.5.1.2 is says i need to configure&amp;nbsp;DMA_ITRIG_INMUX registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The (big) problem is that I can't find this register anywhere. Nor in the reference manual's registers section, nor in the register definitions *.h file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this an error?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any examples using hardware trigger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 May 2020 19:02:01 GMT</pubDate>
    <dc:creator>i_kamal</dc:creator>
    <dc:date>2020-05-23T19:02:01Z</dc:date>
    <item>
      <title>LPC55S69, DMA and DMA_ITRIG_INMUX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067020#M41196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project where i need to read a GPIO port at a fixed frequency (a couple of MHz) and I want to use a DMA triggered by a CTIMER to achieve that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All of which seems totally possible according to reference manual (UM11126).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, when i read chapter 22.5.1.2 is says i need to configure&amp;nbsp;DMA_ITRIG_INMUX registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The (big) problem is that I can't find this register anywhere. Nor in the reference manual's registers section, nor in the register definitions *.h file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this an error?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any examples using hardware trigger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 19:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067020#M41196</guid>
      <dc:creator>i_kamal</dc:creator>
      <dc:date>2020-05-23T19:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69, DMA and DMA_ITRIG_INMUX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067021#M41197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nevermind, i found the answer on chapter 18 (INPUTMUX).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, i'm still interested in an example if someone has one though...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 19:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067021#M41197</guid>
      <dc:creator>i_kamal</dc:creator>
      <dc:date>2020-05-23T19:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69, DMA and DMA_ITRIG_INMUX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067022#M41198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ibrahim,&lt;/P&gt;&lt;P&gt;I have not found the example that the external signal triggers DMA to transfer in SDK package.&lt;/P&gt;&lt;P&gt;I will try to develop an example later if I have time.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 06:26:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067022#M41198</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-05-25T06:26:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69, DMA and DMA_ITRIG_INMUX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067023#M41199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That would be great! Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 09:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-DMA-and-DMA-ITRIG-INMUX/m-p/1067023#M41199</guid>
      <dc:creator>i_kamal</dc:creator>
      <dc:date>2020-05-25T09:10:53Z</dc:date>
    </item>
  </channel>
</rss>