<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックreading data from Grideye Sensor</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-data-from-Grideye-Sensor/m-p/1066590#M41190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been working on this project to read the data from Grideye Sensor which is interfaced with LPC1768 via I2C. but I do not receive any data. when I debugged it probably don't even enter the start condition. can someone help me? ( the program is a Bootloader program and within this program, I am working on Grideye)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jul 2020 10:36:35 GMT</pubDate>
    <dc:creator>poojafsingh</dc:creator>
    <dc:date>2020-07-20T10:36:35Z</dc:date>
    <item>
      <title>reading data from Grideye Sensor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-data-from-Grideye-Sensor/m-p/1066590#M41190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been working on this project to read the data from Grideye Sensor which is interfaced with LPC1768 via I2C. but I do not receive any data. when I debugged it probably don't even enter the start condition. can someone help me? ( the program is a Bootloader program and within this program, I am working on Grideye)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 10:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/reading-data-from-Grideye-Sensor/m-p/1066590#M41190</guid>
      <dc:creator>poojafsingh</dc:creator>
      <dc:date>2020-07-20T10:36:35Z</dc:date>
    </item>
    <item>
      <title>Re: reading data from Grideye Sensor</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-data-from-Grideye-Sensor/m-p/1066591#M41191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="358410" data-username="poojafsingh@gmail.com" href="https://community.nxp.com/people/poojafsingh@gmail.com"&gt;pooja singh&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Are you using the LPCOpen Libraries? There you can find an example of the i2c module to be used as a reference. You need to be sure that the i2c module is well initialized in order to transfer/receive successfully through the bus.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Best regards,&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 17:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/reading-data-from-Grideye-Sensor/m-p/1066591#M41191</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-07-22T17:53:16Z</dc:date>
    </item>
  </channel>
</rss>