<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Hi-speed USB transfer LPC4337</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-speed-USB-transfer-LPC4337/m-p/1064583#M41125</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Sven&lt;/P&gt;&lt;P&gt;Which usb interface do you work with? if USB0, it maximal is 12Mbps. if you want higher speed, use USB1 which is high speed USB device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 May 2020 09:21:32 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2020-05-25T09:21:32Z</dc:date>
    <item>
      <title>Hi-speed USB transfer LPC4337</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-speed-USB-transfer-LPC4337/m-p/1064582#M41124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to make a "high speed" data acquisition board using LPC4337. I have found vcom example, and while it does connect to the PC and shows max speed to be around 12Mbit/s, it only allows me to connect&amp;nbsp;through serial port with speed up to 1843200 baud. Even then I get most of packets lost if I force the transfer in one bulk. VCom driver is probably badly written..&lt;/P&gt;&lt;P&gt;Before going into endeavour of debugging and fixing the vcom, is there any other way of getting higher transfer rates ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would need around 1MB/s, so closely to max theoretical of that 12Mbit/s.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 May 2020 13:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-speed-USB-transfer-LPC4337/m-p/1064582#M41124</guid>
      <dc:creator>svensavic</dc:creator>
      <dc:date>2020-05-24T13:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Hi-speed USB transfer LPC4337</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-speed-USB-transfer-LPC4337/m-p/1064583#M41125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Sven&lt;/P&gt;&lt;P&gt;Which usb interface do you work with? if USB0, it maximal is 12Mbps. if you want higher speed, use USB1 which is high speed USB device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 09:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hi-speed-USB-transfer-LPC4337/m-p/1064583#M41125</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-05-25T09:21:32Z</dc:date>
    </item>
  </channel>
</rss>