<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55xx: Specifications internal reference voltage in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063677#M41060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from table 706 in the user manual (UM11126) I get that the ADC can measure a 1V reference voltage ("Bias_vref_1v from aux_bias module").&lt;/P&gt;&lt;P&gt;I would like to use it, but I can't find any specification for it in the datasheet (e.g. voltage tolerance and temperature dependency).&lt;/P&gt;&lt;P&gt;Wher can I find those specs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also from&amp;nbsp;the SDK I get that bit 1 of the PDRUNCFG0 is used to disable/enable power to this&amp;nbsp;bias voltage, however in table 291 of the user manual this bit is said to be reserved, and bit 19 should be used.&lt;/P&gt;&lt;P&gt;The SDK says that bit 19 is for&amp;nbsp;LDOGPADC...&lt;/P&gt;&lt;P&gt;SDK says bit 15 is for&amp;nbsp;GPADC, the user manual says this bit is also reserved.&lt;/P&gt;&lt;P&gt;All in all I'm a bit puzzled which bits I should use to get the ADC and reference voltage working.&lt;/P&gt;&lt;P&gt;Can someone explain how to use the reference voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Jul 2020 09:26:15 GMT</pubDate>
    <dc:creator>janpieterderuit</dc:creator>
    <dc:date>2020-07-18T09:26:15Z</dc:date>
    <item>
      <title>LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063677#M41060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from table 706 in the user manual (UM11126) I get that the ADC can measure a 1V reference voltage ("Bias_vref_1v from aux_bias module").&lt;/P&gt;&lt;P&gt;I would like to use it, but I can't find any specification for it in the datasheet (e.g. voltage tolerance and temperature dependency).&lt;/P&gt;&lt;P&gt;Wher can I find those specs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also from&amp;nbsp;the SDK I get that bit 1 of the PDRUNCFG0 is used to disable/enable power to this&amp;nbsp;bias voltage, however in table 291 of the user manual this bit is said to be reserved, and bit 19 should be used.&lt;/P&gt;&lt;P&gt;The SDK says that bit 19 is for&amp;nbsp;LDOGPADC...&lt;/P&gt;&lt;P&gt;SDK says bit 15 is for&amp;nbsp;GPADC, the user manual says this bit is also reserved.&lt;/P&gt;&lt;P&gt;All in all I'm a bit puzzled which bits I should use to get the ADC and reference voltage working.&lt;/P&gt;&lt;P&gt;Can someone explain how to use the reference voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jul 2020 09:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063677#M41060</guid>
      <dc:creator>janpieterderuit</dc:creator>
      <dc:date>2020-07-18T09:26:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063678#M41061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan,&lt;/P&gt;&lt;P&gt;what the Um said is vague, I have asked the AE team, I will answer you after I get a feedback.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 04:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063678#M41061</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-07-20T04:51:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063679#M41062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Xiangjun,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Do you have any update on this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 04:13:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063679#M41062</guid>
      <dc:creator>janpieterderuit</dc:creator>
      <dc:date>2020-08-06T04:13:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063680#M41063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jan,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BIAS_VREF_1V is 1.5% accuracy over working voltage and temperature range.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 03:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063680#M41063</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-08-10T03:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063681#M41064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan,&lt;/P&gt;&lt;P&gt;The bit 19 in PDRUNCFG0 for LPC55S69 can control the &lt;SPAN style="font-size: 11.0pt;"&gt;BIAS_VREF_1V&lt;/SPAN&gt;. For accuracy of testing the 1V voltage reference,&amp;nbsp; user have to choose the two options for the ADC converter:&lt;/P&gt;&lt;P&gt;g_LpadcCommandConfigStruct.sampleTimeMode = kLPADC_SampleTimeADCK131;&lt;BR /&gt;g_LpadcCommandConfigStruct.hardwareAverageMode = kLPADC_HardwareAverageCount128;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As my colleague Jennie said that the voltage reference can reach up to 1.5% accuracy with above options&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt; over working voltage and temperature range.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;Hope it can help&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2020 06:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063681#M41064</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-08-13T06:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063682#M41065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;XiangJun,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;thanks for your response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Will the datasheet/User Manual be updated with this info?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jan Pieter&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2020 13:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063682#M41065</guid>
      <dc:creator>janpieterderuit</dc:creator>
      <dc:date>2020-08-17T13:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063683#M41066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jan,&lt;/P&gt;&lt;P&gt;I have notified the AE team of updating the &lt;SPAN style="font-size: 11.0pt;"&gt;BIAS_VREF_1V&lt;/SPAN&gt; part in the UM for LPC55xx family.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 07:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063683#M41066</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-08-18T07:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063684#M41067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 20:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1063684#M41067</guid>
      <dc:creator>janpieterderuit</dc:creator>
      <dc:date>2020-08-18T20:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx: Specifications internal reference voltage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1377715#M47131</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is it exactly 1.0V?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Mirco&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 16:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-Specifications-internal-reference-voltage/m-p/1377715#M47131</guid>
      <dc:creator>mse_videotec</dc:creator>
      <dc:date>2021-11-26T16:18:42Z</dc:date>
    </item>
  </channel>
</rss>