<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Recover from CanBus fault in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Recover-from-CanBus-fault/m-p/1062609#M41009</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What's the best way to get the CANbus going again after it has stopped?&lt;/P&gt;&lt;P&gt;Example - customer disconnects the CAN cable - CANbus interface detects the fault and stops. What is the best way to restart it without having to restart the program from hardware reset?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2020 09:26:09 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2020-04-22T09:26:09Z</dc:date>
    <item>
      <title>Recover from CanBus fault</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Recover-from-CanBus-fault/m-p/1062609#M41009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What's the best way to get the CANbus going again after it has stopped?&lt;/P&gt;&lt;P&gt;Example - customer disconnects the CAN cable - CANbus interface detects the fault and stops. What is the best way to restart it without having to restart the program from hardware reset?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 09:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Recover-from-CanBus-fault/m-p/1062609#M41009</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2020-04-22T09:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: Recover from CanBus fault</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Recover-from-CanBus-fault/m-p/1062610#M41010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ian,&lt;/P&gt;&lt;P&gt;I suppose that you use LPC175x, if it is the case, you can reset only the CAN module with the bit CCAN_RST bit, in other words, you can set the bit, then clear the bit, the CAN module&amp;nbsp; will be reset, then you can reinitialize the CAN module.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61399iEBA61E071A141F47/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 05:20:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Recover-from-CanBus-fault/m-p/1062610#M41010</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-04-23T05:20:15Z</dc:date>
    </item>
  </channel>
</rss>