<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHow to force USB1 peripheral to only use full speed?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537#M41005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering if there is a way to force the USB1 peripheral in device mode to only use full-speed operation.&amp;nbsp; I understand normally the host signals this, and the USB1 peripheral is capable of using full-speed or high-speed, but is there a way to force it to _only_ use full-speed even when the host is high-speed capable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed in the host controller peripheral, it has a field for setting the speed of USB1, but it doesn't work when the device controller is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also understand there is a USB0 peripheral that is full-speed only, but is there a way to force the usb1 peripheral to be full-speed only too in device operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2020 16:12:34 GMT</pubDate>
    <dc:creator>cp1</dc:creator>
    <dc:date>2020-05-22T16:12:34Z</dc:date>
    <item>
      <title>How to force USB1 peripheral to only use full speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537#M41005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering if there is a way to force the USB1 peripheral in device mode to only use full-speed operation.&amp;nbsp; I understand normally the host signals this, and the USB1 peripheral is capable of using full-speed or high-speed, but is there a way to force it to _only_ use full-speed even when the host is high-speed capable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed in the host controller peripheral, it has a field for setting the speed of USB1, but it doesn't work when the device controller is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also understand there is a USB0 peripheral that is full-speed only, but is there a way to force the usb1 peripheral to be full-speed only too in device operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 16:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062537#M41005</guid>
      <dc:creator>cp1</dc:creator>
      <dc:date>2020-05-22T16:12:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to force USB1 peripheral to only use full speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062539#M41007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick reply.&amp;nbsp; Are you sure?&amp;nbsp; It says in the UM that there is "Low-speed (LS), Full-Speed (FS), and High-Speed (HS) support.", in "45.2 Features".&amp;nbsp; So it isn't just highspeed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Conor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 04:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062539#M41007</guid>
      <dc:creator>cp1</dc:creator>
      <dc:date>2020-05-25T04:04:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to force USB1 peripheral to only use full speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062538#M41006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;SPAN style="color: #646464; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="358591" data-username="cp@solokeys.com" href="https://community.nxp.com/people/cp@solokeys.com" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;Conor Patrick&lt;/A&gt;&lt;SPAN style="color: #646464; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;USB1 can only work in high speed. No way to force it work in full speed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2020 03:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1062538#M41006</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-05-25T03:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: How to force USB1 peripheral to only use full speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1178465#M42784</link>
      <description>&lt;P&gt;Sorry for wrong reply....&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 04:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-force-USB1-peripheral-to-only-use-full-speed/m-p/1178465#M42784</guid>
      <dc:creator>namsu_mun</dc:creator>
      <dc:date>2020-11-05T04:13:07Z</dc:date>
    </item>
  </channel>
</rss>