<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLCP540 to LPC546 - Pin compatibility</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057174#M40926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;according to the NXP website LPC540 and LPC546 are pin compatible. I also checked the pin mapping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the MCU professionally reworked from LPC540 to LPC546.&lt;BR /&gt;My PCB is not working properly anymore now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I can not talk to the MCU any more. The IDE cannot discover a target.&lt;BR /&gt;2. The power nets seem to be damaged. I can measure VCC vs GND as 3.3V. Some other nets that are connected to the MCU are on 0.9V, which they were not before.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test:&lt;BR /&gt;1. Visual inspection: No obvious shorted nets.&lt;BR /&gt;2. Electrical tests: An external power supply draws 40 mA, which seems to be correct for the PCB.&lt;/P&gt;&lt;P&gt;3. A multi-meter indicates that there is a short between GND and VCC pins of the MCU.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;My main question is: Is LPC540 and LPC546 truly compatible? That is, can I just switch them out on a PCB?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Jana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 May 2020 19:28:59 GMT</pubDate>
    <dc:creator>jana_beck</dc:creator>
    <dc:date>2020-05-21T19:28:59Z</dc:date>
    <item>
      <title>LCP540 to LPC546 - Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057174#M40926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;according to the NXP website LPC540 and LPC546 are pin compatible. I also checked the pin mapping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the MCU professionally reworked from LPC540 to LPC546.&lt;BR /&gt;My PCB is not working properly anymore now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I can not talk to the MCU any more. The IDE cannot discover a target.&lt;BR /&gt;2. The power nets seem to be damaged. I can measure VCC vs GND as 3.3V. Some other nets that are connected to the MCU are on 0.9V, which they were not before.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test:&lt;BR /&gt;1. Visual inspection: No obvious shorted nets.&lt;BR /&gt;2. Electrical tests: An external power supply draws 40 mA, which seems to be correct for the PCB.&lt;/P&gt;&lt;P&gt;3. A multi-meter indicates that there is a short between GND and VCC pins of the MCU.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;My main question is: Is LPC540 and LPC546 truly compatible? That is, can I just switch them out on a PCB?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Jana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 19:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057174#M40926</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-21T19:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: LCP540 to LPC546 - Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057175#M40927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jana,&lt;/P&gt;&lt;P&gt;To resolve your issue, we need to know your part number of LPC540xx and 546xx. I will check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jennie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 02:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057175#M40927</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-05-22T02:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: LCP540 to LPC546 - Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057176#M40928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;BR /&gt;before:&amp;nbsp;LPC54016JBD100E&lt;BR /&gt;now:&amp;nbsp;LPC54606J512BD100E&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Jana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 03:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057176#M40928</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-22T03:25:00Z</dc:date>
    </item>
    <item>
      <title>Re: LCP540 to LPC546 - Pin compatibility</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057177#M40929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, by checking, this two parts are pin to pin compatible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 03:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP540-to-LPC546-Pin-compatibility/m-p/1057177#M40929</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-05-26T03:33:18Z</dc:date>
    </item>
  </channel>
</rss>