<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: How to start with LPC11A04?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056956#M40921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found that there are differences.&lt;/P&gt;&lt;P&gt;For example for LPC11AX the GPIO base is at&amp;nbsp;&lt;EM&gt;0x50000000&lt;/EM&gt; but for 11U6X is&amp;nbsp;&lt;EM&gt;0xA0000000&lt;/EM&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Apr 2020 05:04:21 GMT</pubDate>
    <dc:creator>csosza</dc:creator>
    <dc:date>2020-04-12T05:04:21Z</dc:date>
    <item>
      <title>How to start with LPC11A04?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056954#M40919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm successfully installed LPCXExpresso v8.2.2 and downloaded&amp;nbsp;lpcopen_3_03_lpcxpresso_lpcxpresso_11e68.zip.&amp;nbsp;&lt;EM&gt;lpc_chip_11u6x&lt;/EM&gt;,&amp;nbsp;&lt;EM&gt;lpc_board_nxp_lpcxpresso_11u68&lt;/EM&gt; and &lt;EM&gt;demos_switch_blinky&lt;/EM&gt; successfully imported and compiled. But I'd like to compile code for LPC11A04. I assume I should have and another &lt;EM&gt;lpc_chip_&amp;lt;..&amp;gt;&lt;/EM&gt; project but I don't how to obtain it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Apr 2020 10:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056954#M40919</guid>
      <dc:creator>csosza</dc:creator>
      <dc:date>2020-04-04T10:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to start with LPC11A04?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056955#M40920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John,&lt;/P&gt;&lt;P&gt;I do not think there is the lpc_chip_11A0x directory, in other words, there is not software package based on LPC11Axx family in LPCOpen. I think the peripheral register address are the same for LPC11U68 and LPC11Axx, so I think you can use the code for LPC11U68 for the LPC11Axx.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2020 07:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056955#M40920</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-04-07T07:31:23Z</dc:date>
    </item>
    <item>
      <title>Re: How to start with LPC11A04?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056956#M40921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found that there are differences.&lt;/P&gt;&lt;P&gt;For example for LPC11AX the GPIO base is at&amp;nbsp;&lt;EM&gt;0x50000000&lt;/EM&gt; but for 11U6X is&amp;nbsp;&lt;EM&gt;0xA0000000&lt;/EM&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Apr 2020 05:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-start-with-LPC11A04/m-p/1056956#M40921</guid>
      <dc:creator>csosza</dc:creator>
      <dc:date>2020-04-12T05:04:21Z</dc:date>
    </item>
  </channel>
</rss>