<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB DFU reference code for LPC55Sxx in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-DFU-reference-code-for-LPC55Sxx/m-p/1053535#M40796</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see there is a DFU USB device library in MCUXpresso, which I could use to add a DFU function to my device.&amp;nbsp; But I think I need to divide the flash into a DFU partition that can be executed while I'm re-flashing the main application partition, and redirect the vector table, etc.&amp;nbsp; Is there reference code for USB DFU for self-flashing on LPC55Sxx?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Aug 2020 18:05:50 GMT</pubDate>
    <dc:creator>mditto1</dc:creator>
    <dc:date>2020-08-03T18:05:50Z</dc:date>
    <item>
      <title>USB DFU reference code for LPC55Sxx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-DFU-reference-code-for-LPC55Sxx/m-p/1053535#M40796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see there is a DFU USB device library in MCUXpresso, which I could use to add a DFU function to my device.&amp;nbsp; But I think I need to divide the flash into a DFU partition that can be executed while I'm re-flashing the main application partition, and redirect the vector table, etc.&amp;nbsp; Is there reference code for USB DFU for self-flashing on LPC55Sxx?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2020 18:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-DFU-reference-code-for-LPC55Sxx/m-p/1053535#M40796</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2020-08-03T18:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU reference code for LPC55Sxx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-DFU-reference-code-for-LPC55Sxx/m-p/1053536#M40797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;-There isn't USB DFU demo under LPC55sxx. There is usb_device_dfu demo under MCUXpresso SDK for LPC54608,&lt;/P&gt;&lt;P&gt;you can have a look.&lt;/P&gt;&lt;P&gt;-And if you just want to update image, you can also make your chip enter into ISP mode, then can through USB , UART or other interface to program, about detail please refer to UM:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109457i3375132C7106DD8B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;-There is a second bootloader , you can have a look, it for lpc55s69.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12327.pdf" title="https://www.nxp.com/docs/en/application-note/AN12327.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12327.pdf&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 03:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-DFU-reference-code-for-LPC55Sxx/m-p/1053536#M40797</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-08-04T03:46:27Z</dc:date>
    </item>
  </channel>
</rss>