<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Programming boot code to external flash for LPC54018</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052764#M40768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm planing for a LPC54018 with an external flash connected on the EMC.&lt;/P&gt;&lt;P&gt;Is there support in the circuit for any ISP and or IAP to program an external flash?&lt;/P&gt;&lt;P&gt;Is there otherwise any tools with support for that? (I've looked at Flashmagic but they don't seem to support the&lt;/P&gt;&lt;P&gt;LPC54018-series) Do you have any sample code for building&amp;nbsp;BootROM functionality?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Göran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2020 16:21:48 GMT</pubDate>
    <dc:creator>goran_lindgren</dc:creator>
    <dc:date>2020-07-16T16:21:48Z</dc:date>
    <item>
      <title>Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052764#M40768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm planing for a LPC54018 with an external flash connected on the EMC.&lt;/P&gt;&lt;P&gt;Is there support in the circuit for any ISP and or IAP to program an external flash?&lt;/P&gt;&lt;P&gt;Is there otherwise any tools with support for that? (I've looked at Flashmagic but they don't seem to support the&lt;/P&gt;&lt;P&gt;LPC54018-series) Do you have any sample code for building&amp;nbsp;BootROM functionality?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Göran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2020 16:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052764#M40768</guid>
      <dc:creator>goran_lindgren</dc:creator>
      <dc:date>2020-07-16T16:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052765#M40769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suggest you refer this article of&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-341559"&gt;How to boot from the external flash for LPC54018&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 07:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052765#M40769</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-07-17T07:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052766#M40770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your answer, but that article doesn’t handle programing of external flash memories connected to the EMC as far as I can see.&lt;/P&gt;&lt;P&gt;Has the Segger software build in functionality to handle truly external flashes as well? (on the screen shoots I can see no reference to that or setup for that)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Göran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 09:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052766#M40770</guid>
      <dc:creator>goran_lindgren</dc:creator>
      <dc:date>2020-07-20T09:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052767#M40771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;do you mean parallel nor?&lt;/P&gt;&lt;P&gt;By checking,&amp;nbsp; we don't have programming tool&amp;nbsp; for it.&lt;/P&gt;&lt;P&gt;for external memory, we suggest use spifi FLASH.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 08:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052767#M40771</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-07-21T08:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052768#M40772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, parallel nor flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information and your swift reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Göran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 10:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052768#M40772</guid>
      <dc:creator>goran_lindgren</dc:creator>
      <dc:date>2020-07-21T10:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: Programming boot code to external flash for LPC54018</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052769#M40773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 01:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-boot-code-to-external-flash-for-LPC54018/m-p/1052769#M40773</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-07-22T01:45:45Z</dc:date>
    </item>
  </channel>
</rss>