<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5526 9bit uart multiprocessor setup in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-9bit-uart-multiprocessor-setup/m-p/1051205#M40729</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jeroen,&lt;/P&gt;&lt;P&gt;I agree with you that the usart driver does not have any declaration, macro, enums for the 9 bits data support, but the hardware of USART module supports 9 bits data format.&lt;/P&gt;&lt;P&gt;This is the USART FIFO registers, obviously, it supports 9 bits data, the bits is from 0 to 8, the total is 9 bits.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22987iD23420299536194E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 May 2020 05:29:03 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-05-07T05:29:03Z</dc:date>
    <item>
      <title>LPC5526 9bit uart multiprocessor setup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-9bit-uart-multiprocessor-setup/m-p/1051204#M40728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using a LPC5526 and I want to setup 9bit UART (RS485)&amp;nbsp; communication, the 9th bit is used for the address detection.&lt;/P&gt;&lt;P&gt;The manual states that the CPU should be capable of 9bit multiprocessor:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107676i1BCD5A8A2F0531FA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Only in the GUI peripheral setup there no option to choose it, also in the fsl_usart.h file there a no enums / functions to configure this. Im using the 2.1.1 driver from the SDK.#&lt;/P&gt;&lt;P&gt;Do I look in the wrong place or are these options not available in the driver library?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 13:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-9bit-uart-multiprocessor-setup/m-p/1051204#M40728</guid>
      <dc:creator>jeroenbussink</dc:creator>
      <dc:date>2020-05-06T13:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5526 9bit uart multiprocessor setup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-9bit-uart-multiprocessor-setup/m-p/1051205#M40729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jeroen,&lt;/P&gt;&lt;P&gt;I agree with you that the usart driver does not have any declaration, macro, enums for the 9 bits data support, but the hardware of USART module supports 9 bits data format.&lt;/P&gt;&lt;P&gt;This is the USART FIFO registers, obviously, it supports 9 bits data, the bits is from 0 to 8, the total is 9 bits.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22987iD23420299536194E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2020 05:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-9bit-uart-multiprocessor-setup/m-p/1051205#M40729</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-05-07T05:29:03Z</dc:date>
    </item>
  </channel>
</rss>