<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54628 Brownout Interrupt Detection in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-Brownout-Interrupt-Detection/m-p/1051069#M40718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with brownout interrupt detection on LPC54628.&lt;/P&gt;&lt;P&gt;Lowering the VDD level to the BOD interrupt level triggers the interrupt.&lt;/P&gt;&lt;P&gt;However the interrupt is constantly triggered while I am on this level (i.e. VDD = BOD interrupt level).&lt;/P&gt;&lt;P&gt;Is this the way BOD interrupt is intended to work?&lt;/P&gt;&lt;P&gt;The BOD interrupt can clog up my MCU load and I cannot handle anything while the VDD level is on the BOD interrupt level.&lt;/P&gt;&lt;P&gt;Is it possible to configure LPC54628 to trigger the BOD interrupt only once and not constantly while &lt;SPAN&gt;VDD = BOD interrupt level&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2020 07:57:01 GMT</pubDate>
    <dc:creator>danielgull</dc:creator>
    <dc:date>2020-07-02T07:57:01Z</dc:date>
    <item>
      <title>LPC54628 Brownout Interrupt Detection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-Brownout-Interrupt-Detection/m-p/1051069#M40718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with brownout interrupt detection on LPC54628.&lt;/P&gt;&lt;P&gt;Lowering the VDD level to the BOD interrupt level triggers the interrupt.&lt;/P&gt;&lt;P&gt;However the interrupt is constantly triggered while I am on this level (i.e. VDD = BOD interrupt level).&lt;/P&gt;&lt;P&gt;Is this the way BOD interrupt is intended to work?&lt;/P&gt;&lt;P&gt;The BOD interrupt can clog up my MCU load and I cannot handle anything while the VDD level is on the BOD interrupt level.&lt;/P&gt;&lt;P&gt;Is it possible to configure LPC54628 to trigger the BOD interrupt only once and not constantly while &lt;SPAN&gt;VDD = BOD interrupt level&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 07:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-Brownout-Interrupt-Detection/m-p/1051069#M40718</guid>
      <dc:creator>danielgull</dc:creator>
      <dc:date>2020-07-02T07:57:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54628 Brownout Interrupt Detection</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-Brownout-Interrupt-Detection/m-p/1051070#M40719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;Hi, Daniel,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;I guess that you do not clear the &lt;/SPAN&gt;BODINTSTAT bit in BOD control register (BODCTR) in your BOD ISR, if you do not clear the bit, the ISR will be entered again and again.&lt;BR clear="none" /&gt; The BODINTSTAT bit can be cleared by writing a 1 to the bit.&lt;BR clear="none" /&gt; For detailed inf, pls refer to section 4.5.108 BOD control register in UM10912.pdf.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114420iC2172AA893E957AE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 13:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-Brownout-Interrupt-Detection/m-p/1051070#M40719</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-07-02T13:55:57Z</dc:date>
    </item>
  </channel>
</rss>