<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Unique ID of LPC4357</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047540#M40610</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you read carefully the description of the words in Table 14, you see that the unique ID applies only to the flashless parts, e.g. LPC4350. For parts with on-chip flash, e.g. the LPC4357 these 4 word locations are "reserved".&lt;/P&gt;&lt;P&gt;For the flash parts there is an IAP command to read a serial number.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Apr 2020 08:19:10 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2020-04-17T08:19:10Z</dc:date>
    <item>
      <title>Unique ID of LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047539#M40609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read a unique id of LPC4357 which is 128 bit long(specified in the user manual). But I can't find the address from where I should read it. The user manual has no mention of this thing clearly apart from just telling that it has 128-bit unique id.&amp;nbsp;&lt;A class="link-titled" href="https://www.y-ic.es/datasheet/e0/(2).pdf" title="https://www.y-ic.es/datasheet/e0/(2).pdf"&gt;https://www.y-ic.es/datasheet/e0/(2).pdf&lt;/A&gt;&amp;nbsp; This user manual states in chapter 4.4 at address&amp;nbsp; 0x4004 5000 there is a unique id but using MCU expresso when I see that memory location the id is not 128 bit long. I have attached data available at the given memory address. In STM32 there is a similar unique id of 96 bits located at a flash address which once can read easily but in LPC4357 it is difficult as manual doesn't provide adequate information. Please help me in reading the unique id of the processor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 06:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047539#M40609</guid>
      <dc:creator>hdhedhu</dc:creator>
      <dc:date>2020-04-17T06:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: Unique ID of LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047540#M40610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you read carefully the description of the words in Table 14, you see that the unique ID applies only to the flashless parts, e.g. LPC4350. For parts with on-chip flash, e.g. the LPC4357 these 4 word locations are "reserved".&lt;/P&gt;&lt;P&gt;For the flash parts there is an IAP command to read a serial number.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 08:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047540#M40610</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-04-17T08:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: Unique ID of LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047541#M40611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Bernhard Fink&lt;/P&gt;&lt;P&gt;Using chip library inbuild function&amp;nbsp;Chip_IAP_ReadUID I am able to read unique id.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2020 07:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Unique-ID-of-LPC4357/m-p/1047541#M40611</guid>
      <dc:creator>hdhedhu</dc:creator>
      <dc:date>2020-04-18T07:31:56Z</dc:date>
    </item>
  </channel>
</rss>