<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPIFI code execution on LPCXpresso54608 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046626#M40591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to solve my problem. SPIFI was not put in memory mode. for others that might have the same problem, i had to add SPIFI_SetMemoryCommand before the memory could be accessed trough AHB after setting up the peripheral. you can find the example in the SDK - flash_component_nor_spifi. the difference with the example is that the read function actually resets the memory mode after reading it using memcpy, and we don't want that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2020 16:00:26 GMT</pubDate>
    <dc:creator>alexis_marquet</dc:creator>
    <dc:date>2020-06-16T16:00:26Z</dc:date>
    <item>
      <title>SPIFI code execution on LPCXpresso54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046625#M40590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI, I'm having trouble running code from spifi flash on the LPCXpresso546XX, specifically the 54608 version. When placing code in internal flash, the program runs fine, but when i added *(.text) -&amp;gt; Board flash, the program hardfaults with a IBUSERR. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far the resources i have found about this were mostly about the SPIFI driver used to program the flash with the debugger. I am wondering what (if any) configuration of the SPIFI is needed in order to run the code from external flash on the development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd be happy to supply more info as needed, my only idea so far is that maybe there needs to be some configuration about timing when using the SPIFI device mapped to AHB bus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope you can help me,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexis Marquet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: The EmWin tools/ appwizard is not up to the last version on your website, which is still giving 6.10f while last version is 6.14a: &lt;A class="link-titled" href="https://forum.segger.com/index.php/Thread/7257-ROM-usage-of-Appwizard/#post26665" title="https://forum.segger.com/index.php/Thread/7257-ROM-usage-of-Appwizard/#post26665"&gt;ROM usage of Appwizard - emWin related - SEGGER - Forum&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2020 11:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046625#M40590</guid>
      <dc:creator>alexis_marquet</dc:creator>
      <dc:date>2020-06-15T11:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: SPIFI code execution on LPCXpresso54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046626#M40591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to solve my problem. SPIFI was not put in memory mode. for others that might have the same problem, i had to add SPIFI_SetMemoryCommand before the memory could be accessed trough AHB after setting up the peripheral. you can find the example in the SDK - flash_component_nor_spifi. the difference with the example is that the read function actually resets the memory mode after reading it using memcpy, and we don't want that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 16:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046626#M40591</guid>
      <dc:creator>alexis_marquet</dc:creator>
      <dc:date>2020-06-16T16:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: SPIFI code execution on LPCXpresso54608</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046627#M40592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alexis,&lt;/P&gt;&lt;P&gt;You can also find spifi demo under SDK,download from &lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113027i6852EF23FB7B460A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 07:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SPIFI-code-execution-on-LPCXpresso54608/m-p/1046627#M40592</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-06-17T07:44:19Z</dc:date>
    </item>
  </channel>
</rss>