<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: provide gigabit Ethernet on LPC4370</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/provide-gigabit-Ethernet-on-LPC4370/m-p/1046288#M40589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The interface with the highest throughput is the SDRAM interface. You can use an FPGA connected to this interface and convert it to gigabit ethernet. But I assume that this is expensive and and a lot of work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SGPIO interface is also pretty fast if you configure it for a 16-bit parallel output, this would be on the FPGA side a little bit easier to realize, but also here you have the cost and the development work on the FPGA side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then comes the LCD interface, 24-bit wide, also a relatively high throughput when you clock it on 50MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2020 08:33:21 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2020-05-20T08:33:21Z</dc:date>
    <item>
      <title>provide gigabit Ethernet on LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/provide-gigabit-Ethernet-on-LPC4370/m-p/1046287#M40588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using lpc-link2 (lpc4370) for a project which uses ADC in 60MHz(need 120MB/s for transfer). regarding the datasheet there is no serial protocol that can support this speed. there may be a solution that i can use an interface and send data in parallel then use for example gigabit ethernet rather than fast ethernet, however I don't know how! do you guys have any suggestion? thanks in advance for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 05:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/provide-gigabit-Ethernet-on-LPC4370/m-p/1046287#M40588</guid>
      <dc:creator>navidfanaee</dc:creator>
      <dc:date>2020-05-20T05:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: provide gigabit Ethernet on LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/provide-gigabit-Ethernet-on-LPC4370/m-p/1046288#M40589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The interface with the highest throughput is the SDRAM interface. You can use an FPGA connected to this interface and convert it to gigabit ethernet. But I assume that this is expensive and and a lot of work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SGPIO interface is also pretty fast if you configure it for a 16-bit parallel output, this would be on the FPGA side a little bit easier to realize, but also here you have the cost and the development work on the FPGA side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then comes the LCD interface, 24-bit wide, also a relatively high throughput when you clock it on 50MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 08:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/provide-gigabit-Ethernet-on-LPC4370/m-p/1046288#M40589</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-05-20T08:33:21Z</dc:date>
    </item>
  </channel>
</rss>