<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54x USB VBUS when Vdd=0V</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54x-USB-VBUS-when-Vdd-0V/m-p/1043730#M40521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, David,&lt;/P&gt;&lt;P&gt;I think the requirement of reduction of USB_VBUS voltage is correct when the VDD is zero while the USB_VBUS voltage is coming.&lt;/P&gt;&lt;P&gt;Regarding the LPCXpresso54628 Development Board&amp;nbsp;(OM13098), as you know that the board OM13098 is always bus-powered device, in other words, once the USB port is inserted, the LPC54xxx will be powered immediately by the USB_VBUS, so the resistor divider for USB_VBUS does not make sense.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jun 2020 03:13:22 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-06-03T03:13:22Z</dc:date>
    <item>
      <title>LPC54x USB VBUS when Vdd=0V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54x-USB-VBUS-when-Vdd-0V/m-p/1043729#M40520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is an incorrect&amp;nbsp;specification&amp;nbsp;in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/LPC546XX.pdf"&gt;LPC546XX Product Data Sheet (Rev. 2.7) &lt;/A&gt;document in Section 13.7 "Suggested USB0 Full-speed interface solutions" (pg151). It is suggested to use a voltage divider to lower the voltage on the pin to below 3.6V when Vdd = 0V and VBUS is present.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet states:&amp;nbsp;"&lt;EM&gt;the voltage divider should provide a reduction of 3.6 V/5.25 V or ~0.686 V&lt;/EM&gt;".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This looks incorrect, the &lt;STRONG&gt;ratio&lt;/STRONG&gt;&amp;nbsp;should be 0.686, and the&lt;STRONG&gt;&amp;nbsp;reduction&lt;/STRONG&gt;&amp;nbsp;should be at least 1.65V (=5.25-3.6).&lt;/P&gt;&lt;P&gt;Furthermore, the ratios on the LPCXpresso54628 Development Board&amp;nbsp;(OM13098) look incorrect, it uses R3=470 and R4=2.2k divider which results in an output voltage of 4.326V for a 5.25V VBUS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am i missing something here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Related thread:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/499375"&gt;What is are the resistor values permitted on Vbus for the LPC1837&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2020 20:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54x-USB-VBUS-when-Vdd-0V/m-p/1043729#M40520</guid>
      <dc:creator>nudge</dc:creator>
      <dc:date>2020-06-01T20:57:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54x USB VBUS when Vdd=0V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54x-USB-VBUS-when-Vdd-0V/m-p/1043730#M40521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, David,&lt;/P&gt;&lt;P&gt;I think the requirement of reduction of USB_VBUS voltage is correct when the VDD is zero while the USB_VBUS voltage is coming.&lt;/P&gt;&lt;P&gt;Regarding the LPCXpresso54628 Development Board&amp;nbsp;(OM13098), as you know that the board OM13098 is always bus-powered device, in other words, once the USB port is inserted, the LPC54xxx will be powered immediately by the USB_VBUS, so the resistor divider for USB_VBUS does not make sense.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 03:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54x-USB-VBUS-when-Vdd-0V/m-p/1043730#M40521</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-06-03T03:13:22Z</dc:date>
    </item>
  </channel>
</rss>