<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: dual bootloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/dual-bootloader/m-p/1043467#M40519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;- From your picture, it seems the UART haven't communicate well, please check Device Manage to confirm&lt;/P&gt;&lt;P&gt;it COM7, and fist just try command &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; blhost.exe -p COM7 get-property 1&lt;/P&gt;&lt;P&gt;- If you just want to update apps, you can directly use blhost to download when your chip entered ISP mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2020 06:21:06 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2020-06-02T06:21:06Z</dc:date>
    <item>
      <title>dual bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/dual-bootloader/m-p/1043466#M40518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, recently when I am modifying the verision of image referring to&amp;nbsp;AN12327SW and the AN12327.After I excute this steps " Close the serial terminal. Open bash window or command window and execute flash_program.bat. This script calls blhost.exe and downloads dsbl_app_crc.bin in the Receive Region. Running flash_program.bat need two parameters. First is UART COM index, second is the full name of the app image." It causes an unexpected error shows like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108822iDD961E3DB5A53BCB/image-size/large?v=v2&amp;amp;px=999" title="2d3a3234d12cb23698a9e9edffe64d07_pastedImage_2.png" alt="2d3a3234d12cb23698a9e9edffe64d07_pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So,I have&amp;nbsp;three quetions:&lt;/P&gt;&lt;P&gt;1:How to solve this problem.&lt;/P&gt;&lt;P&gt;2.If I want to modify the version of the image , which step should I do?&lt;/P&gt;&lt;P&gt;3,Is there any other methods to download the new apps to update the images?&lt;/P&gt;&lt;P&gt;This questions pullze me long time ,I hope you can help me.Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 03:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/dual-bootloader/m-p/1043466#M40518</guid>
      <dc:creator>zhangeh10594</dc:creator>
      <dc:date>2020-06-02T03:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: dual bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/dual-bootloader/m-p/1043467#M40519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;- From your picture, it seems the UART haven't communicate well, please check Device Manage to confirm&lt;/P&gt;&lt;P&gt;it COM7, and fist just try command &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; blhost.exe -p COM7 get-property 1&lt;/P&gt;&lt;P&gt;- If you just want to update apps, you can directly use blhost to download when your chip entered ISP mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 06:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/dual-bootloader/m-p/1043467#M40519</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-06-02T06:21:06Z</dc:date>
    </item>
  </channel>
</rss>