<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54618 and RTC Battery power consumption</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039151#M40438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun Rong,&lt;/P&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;I measured the current that flows on JP13 (with board not powered) and it is 34.6uA (microampere).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I disconnect R33 current absorbtion is about 0.3uA. But, how can i leave floating a RESET pin?? Datasheet says that there is an internal pull-up, but I would feel more comfortable with an external reset supervisor. &lt;BR /&gt;So, how could I connect the MCP809 to avoid current consumption?&lt;/P&gt;&lt;P&gt;Thanks in advance for any response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 May 2020 14:58:49 GMT</pubDate>
    <dc:creator>m_dibiaggio</dc:creator>
    <dc:date>2020-05-21T14:58:49Z</dc:date>
    <item>
      <title>LPC54618 and RTC Battery power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039149#M40436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I have a problem with power consumption of LPC54618 RTC. As illustrated in attached PDF I have a board with the configuration visible on the schematic. Battery is a rechargeable Panasonic VL-1220 with 7mA/h current capacitance. LPC54618 datasheet reports that, in power off conditions (board off, with only VBAT present), consumption is 340nA. I can't measure precisely the consumption, but after several tests, I see that the current absorbed from RTC is more than that indicated. I tried to left reset pin floating ad suggested in the datasheet, but without significative differences (and how can I left floating a reset pin?!?!). I have 2 different boards with same LPC54618 RTC circuit and same problem.&lt;/P&gt;&lt;P&gt;Is there anyone that can help me to understand how solve this problem?&lt;/P&gt;&lt;P&gt;For information I used same battery on LPC1768 controller (that has similar consumption characteristics) without problems and duration about 6 months.&lt;/P&gt;&lt;P&gt;Many thanks in advance for any information.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Marco Di Biaggio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2020 05:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039149#M40436</guid>
      <dc:creator>m_dibiaggio</dc:creator>
      <dc:date>2020-05-04T05:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618 and RTC Battery power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039150#M40437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Marco,&lt;/P&gt;&lt;P&gt;I suggest you use a precise Multi Meter Instrument to test the RTC pin current with VDD=VDDA=VREFP=GND, you can not figure out the RTC current by battery energy consumption for a fixed&amp;nbsp; time, because the battery has large leakage current, in other words, battery consumes power itself.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2020 03:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039150#M40437</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-05-08T03:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618 and RTC Battery power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039151#M40438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun Rong,&lt;/P&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;I measured the current that flows on JP13 (with board not powered) and it is 34.6uA (microampere).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I disconnect R33 current absorbtion is about 0.3uA. But, how can i leave floating a RESET pin?? Datasheet says that there is an internal pull-up, but I would feel more comfortable with an external reset supervisor. &lt;BR /&gt;So, how could I connect the MCP809 to avoid current consumption?&lt;/P&gt;&lt;P&gt;Thanks in advance for any response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 14:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039151#M40438</guid>
      <dc:creator>m_dibiaggio</dc:creator>
      <dc:date>2020-05-21T14:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54618 and RTC Battery power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039152#M40439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Resetn pin floating means that there is not any connection on the pin Resetn or any driven signal.&lt;/P&gt;&lt;P&gt;I have checked your prb_Battery_r0.pdf file, if you connect the MCP809, when the MCP809 is power off, you can not guarantee that the /RST pin of MCP809 is float in the case.&lt;/P&gt;&lt;P&gt;As an alternative, if you replace the R33 with a diode, what is the result? I am not sure if it can solve your issue with a diode, pls have a try.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 03:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54618-and-RTC-Battery-power-consumption/m-p/1039152#M40439</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-05-22T03:27:41Z</dc:date>
    </item>
  </channel>
</rss>