<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I verify external 50 MHz crystal with LPC540? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036694#M40356</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jun,&lt;BR /&gt;thank you for the reply.&lt;BR /&gt;I am actually trying to do it the other way around, having an external clock (which is only used by another component, to be precise by a PHY) and verifying if the clock signal is correct with the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to have a functional test for my electronic assembly with as much measurements done using the MCU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Mar 2020 02:11:00 GMT</pubDate>
    <dc:creator>jana_beck</dc:creator>
    <dc:date>2020-03-20T02:11:00Z</dc:date>
    <item>
      <title>Can I verify external 50 MHz crystal with LPC540?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036692#M40354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;BR /&gt;I am currently working on setting up a functional test for my application.&lt;BR /&gt;For one of the components I need a 50 MHz clock signal.&lt;BR /&gt;Is it possible to measure if this clock signal is correct using my MCU (LPC54016JBD100).&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I am not very familiar with internal clocks, any help appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2020 18:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036692#M40354</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-03-16T18:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: Can I verify external 50 MHz crystal with LPC540?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036693#M40355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Jana&lt;/P&gt;&lt;P&gt;We can measure CLKOUT pin to check internal clock.&lt;/P&gt;&lt;P&gt;Using CLKOUTSELA to set the clock source.&lt;/P&gt;&lt;P&gt;Below diagram, main_clk can be measured by CLKOUT pin.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104471i7BE9AEF1C78A5612/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 10:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036693#M40355</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-03-19T10:23:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can I verify external 50 MHz crystal with LPC540?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036694#M40356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jun,&lt;BR /&gt;thank you for the reply.&lt;BR /&gt;I am actually trying to do it the other way around, having an external clock (which is only used by another component, to be precise by a PHY) and verifying if the clock signal is correct with the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to have a functional test for my electronic assembly with as much measurements done using the MCU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 02:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036694#M40356</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-03-20T02:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: Can I verify external 50 MHz crystal with LPC540?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036695#M40357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You want to use LPC to measure an external 50MHz clock.&lt;/P&gt;&lt;P&gt;The idea is to use input capture feature to measure 50M pin. each toggle trigger a capture_counter+1.&lt;/P&gt;&lt;P&gt;You need also have an accurate external low frequency clock (Don't use internal FRO, it has 1% error), for example 100KHz, it trigger interrupt for each clock. then you can calculate "capture_counter" value.&lt;/P&gt;&lt;P&gt;the measured clock = 100Khz * capture_counter value&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 03:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-verify-external-50-MHz-crystal-with-LPC540/m-p/1036695#M40357</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-03-23T03:39:25Z</dc:date>
    </item>
  </channel>
</rss>