<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Mistake in AN12395 regarding pull-up values</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Mistake-in-AN12395-regarding-pull-up-values/m-p/1033284#M40240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I think it is a typo issue here. I will forward to the author.Thanks for your reporting!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Feb 2020 03:29:31 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-02-24T03:29:31Z</dc:date>
    <item>
      <title>Mistake in AN12395 regarding pull-up values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Mistake-in-AN12395-regarding-pull-up-values/m-p/1033283#M40239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Table 2 on page 6 of the file "AN12395-OM-SE050ARD_hardware_overview.pdf" shows that when J37 and J38 are installed in position 1-2 the pull up resistance is 560 Ohms.&amp;nbsp; However, according to the schematic between pages 20 &amp;amp; 21 these (J37 &amp;amp; J38) jumpers insert an 820 Ohm resistor in parallel with the default 3.3K Ohm resistor.&amp;nbsp; This is does not make 560 Ohms but 657 ohms.&amp;nbsp; I also validated this with a multi-meter.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 20:05:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Mistake-in-AN12395-regarding-pull-up-values/m-p/1033283#M40239</guid>
      <dc:creator>720adams</dc:creator>
      <dc:date>2020-02-14T20:05:30Z</dc:date>
    </item>
    <item>
      <title>Re: Mistake in AN12395 regarding pull-up values</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Mistake-in-AN12395-regarding-pull-up-values/m-p/1033284#M40240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I think it is a typo issue here. I will forward to the author.Thanks for your reporting!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 03:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Mistake-in-AN12395-regarding-pull-up-values/m-p/1033284#M40240</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-02-24T03:29:31Z</dc:date>
    </item>
  </channel>
</rss>