<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S69 : 1-bit SPI NOR FLASH support in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032238#M40171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;I get feedback from AE team, the FlexComm3 module is used as single I/O SPI NOR flash interface as the following fig.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/123693i74F40F721AC6E4F7/image-size/large?v=v2&amp;amp;px=999" title="https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png" alt="https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Dec 2019 05:02:41 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-12-12T05:02:41Z</dc:date>
    <item>
      <title>LPC55S69 : 1-bit SPI NOR FLASH support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032236#M40169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In UM mentioned about NOR flash memory support in ROM code directly :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;8.6.11.2 1-bit SPI NOR FLASH support (for version 1B only)&amp;nbsp;&lt;/STRONG&gt;&amp;nbsp; and it can be programmed by using blhost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it is not clear to what SPI interface it can be connected and how to initialize it&amp;nbsp; ( if need ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about ROM api what use used for work with SB file ?&lt;/P&gt;&lt;P&gt;Can they work directly with this NOR memory ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Nov 2019 19:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032236#M40169</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-11-23T19:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : 1-bit SPI NOR FLASH support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032237#M40170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to admit that the part in UM11126.pdf is confused and unclear, I have asked AE team, I will give you a reply after I get a feedback.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 09:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032237#M40170</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-11T09:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : 1-bit SPI NOR FLASH support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032238#M40171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;I get feedback from AE team, the FlexComm3 module is used as single I/O SPI NOR flash interface as the following fig.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/123693i74F40F721AC6E4F7/image-size/large?v=v2&amp;amp;px=999" title="https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png" alt="https___community.nxp.com_servlet_JiveServlet_showImage_2-1244799-293593_pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 05:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-1-bit-SPI-NOR-FLASH-support/m-p/1032238#M40171</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-12T05:02:41Z</dc:date>
    </item>
  </channel>
</rss>