<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Programming flash on a single LPC-Link2 board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-flash-on-a-single-LPC-Link2-board/m-p/1030901#M40124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal&lt;/P&gt;&lt;P&gt;Do you want to program the application burning file to LPC4370 ? You can do that with FlashMagic in LPC4370 ISP mode.&lt;/P&gt;&lt;P&gt;FlashMagic download:&amp;nbsp;&lt;A class="link-titled" href="http://www.flashmagictool.com/" title="http://www.flashmagictool.com/"&gt;Flash Magic - Welcome&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer UM for the LPC4370 ISP mode setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Mar 2020 16:25:23 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2020-03-03T16:25:23Z</dc:date>
    <item>
      <title>Programming flash on a single LPC-Link2 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-flash-on-a-single-LPC-Link2-board/m-p/1030900#M40123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have one LPC-Link2 board (with LPC4370 microcontroller). I found out that it can be used either as a target board or as a debbuger board for a separate&amp;nbsp;target. But, would it be possible just to program flash on a single LPC-Link2 board just to run binary code (without debugging yet) without having to buy an additional LPC-Link2 board?&lt;/P&gt;&lt;P&gt;I tried to program flash with a .bin file (which was an example included with LPC-Scrypt) with LPC-Scrypt tool. That example worked properly on the board (the LED blinked). Later, I created and built a simple LPCXpresso C++ project, but I&amp;nbsp;wasn't able&amp;nbsp;to send it to flash with an appriopriate tool in the IDE. Then, I tried to send the generated .bin or .axf file to flash with LPCScrypt, but it appeared not to work properly on the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Feb 2020 13:57:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-flash-on-a-single-LPC-Link2-board/m-p/1030900#M40123</guid>
      <dc:creator>michj</dc:creator>
      <dc:date>2020-02-29T13:57:38Z</dc:date>
    </item>
    <item>
      <title>Re: Programming flash on a single LPC-Link2 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-flash-on-a-single-LPC-Link2-board/m-p/1030901#M40124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal&lt;/P&gt;&lt;P&gt;Do you want to program the application burning file to LPC4370 ? You can do that with FlashMagic in LPC4370 ISP mode.&lt;/P&gt;&lt;P&gt;FlashMagic download:&amp;nbsp;&lt;A class="link-titled" href="http://www.flashmagictool.com/" title="http://www.flashmagictool.com/"&gt;Flash Magic - Welcome&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refer UM for the LPC4370 ISP mode setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 16:25:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programming-flash-on-a-single-LPC-Link2-board/m-p/1030901#M40124</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-03-03T16:25:23Z</dc:date>
    </item>
  </channel>
</rss>