<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S69 libpower_hardabi.a in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-libpower-hardabi-a/m-p/1027791#M40025</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use&amp;nbsp;lpcxpresso55s69_power_manager_lpc with lpc55s69_evk. I am using SDK 2.7.&amp;nbsp;&lt;/P&gt;&lt;P&gt;sleep mode, deep sleep mode, deep power down mode work well.&lt;/P&gt;&lt;P&gt;But it cannot wake up from power down mode.&lt;/P&gt;&lt;P&gt;I change to use&amp;nbsp;libpower_softabi.a and change the project config, architecture to FPV5-SP-D16(soft ABI), then it can wake up from power down mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the libpower_hardabi.a buggy or do I need to do any extra configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Dec 2019 21:00:34 GMT</pubDate>
    <dc:creator>francisy</dc:creator>
    <dc:date>2019-12-30T21:00:34Z</dc:date>
    <item>
      <title>LPC55S69 libpower_hardabi.a</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-libpower-hardabi-a/m-p/1027791#M40025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use&amp;nbsp;lpcxpresso55s69_power_manager_lpc with lpc55s69_evk. I am using SDK 2.7.&amp;nbsp;&lt;/P&gt;&lt;P&gt;sleep mode, deep sleep mode, deep power down mode work well.&lt;/P&gt;&lt;P&gt;But it cannot wake up from power down mode.&lt;/P&gt;&lt;P&gt;I change to use&amp;nbsp;libpower_softabi.a and change the project config, architecture to FPV5-SP-D16(soft ABI), then it can wake up from power down mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the libpower_hardabi.a buggy or do I need to do any extra configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Dec 2019 21:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-libpower-hardabi-a/m-p/1027791#M40025</guid>
      <dc:creator>francisy</dc:creator>
      <dc:date>2019-12-30T21:00:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 libpower_hardabi.a</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-libpower-hardabi-a/m-p/1027792#M40026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Francis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm how you are attempting to wake up from power down.&lt;/P&gt;&lt;P&gt;I have attempted from my end but it works without any problems using the hardabi library.&lt;/P&gt;&lt;P&gt;I can wake up using the reset or the S1(ISP button).&lt;/P&gt;&lt;P&gt;I am using the SDK 2.7.0 and the LPCXpresso55S69 Rev A1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2020 17:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-libpower-hardabi-a/m-p/1027792#M40026</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-01-03T17:25:35Z</dc:date>
    </item>
  </channel>
</rss>