<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69: crystal-less design</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-crystal-less-design/m-p/1022596#M39934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Nov 2019 15:49:51 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2019-11-25T15:49:51Z</dc:date>
    <item>
      <title>LPC55S69: crystal-less design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-crystal-less-design/m-p/1022595#M39933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I understand right and MCU can be totally crystalless&amp;nbsp; ? And supports whole declared temperature range ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PLL0 can use FRO_12MHz and generate 100 or 150 Mhz clocks without any problems.&lt;/P&gt;&lt;P&gt;SPi and I2C can use FRO_12Mhz for clocking ( SPI speed can be 10Mhz ?).&lt;/P&gt;&lt;P&gt;RTC can own FRO32KHz oscillator but it may be not so precise for keep calendar time.&lt;/P&gt;&lt;P&gt;Is this so ? How to calculate possible drift while 1 week ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be problems if no any crystals is not in use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 12:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-crystal-less-design/m-p/1022595#M39933</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-11-21T12:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: crystal-less design</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-crystal-less-design/m-p/1022596#M39934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 15:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-crystal-less-design/m-p/1022596#M39934</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-11-25T15:49:51Z</dc:date>
    </item>
  </channel>
</rss>