<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックExample code for LPC 4370 in LPC link2</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Example-code-for-LPC-4370-in-LPC-link2/m-p/1020743#M39880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am unable to find the example files for LPC Link2 (LPC 4370). Please share LPC4370_LPCLink2_LEDblinky.zip&lt;/P&gt;&lt;P&gt;This is to test the Link2 board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jan 2020 10:42:01 GMT</pubDate>
    <dc:creator>naveen_b160496e</dc:creator>
    <dc:date>2020-01-30T10:42:01Z</dc:date>
    <item>
      <title>Example code for LPC 4370 in LPC link2</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Example-code-for-LPC-4370-in-LPC-link2/m-p/1020743#M39880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am unable to find the example files for LPC Link2 (LPC 4370). Please share LPC4370_LPCLink2_LEDblinky.zip&lt;/P&gt;&lt;P&gt;This is to test the Link2 board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 10:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Example-code-for-LPC-4370-in-LPC-link2/m-p/1020743#M39880</guid>
      <dc:creator>naveen_b160496e</dc:creator>
      <dc:date>2020-01-30T10:42:01Z</dc:date>
    </item>
    <item>
      <title>Re: Example code for LPC 4370 in LPC link2</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Example-code-for-LPC-4370-in-LPC-link2/m-p/1020744#M39881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Puh, where did you find a reference to this zip file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is a setup which worked one time under LPCXpresso, no idea if it can be imported into MCUXpresso.&lt;/P&gt;&lt;P&gt;It is a quick &amp;amp; dirty derivative of a Blinky project for the LPC4330 Xplorer board from NGX Technologies.&lt;/P&gt;&lt;P&gt;The smaller one is the same blinky function, reduced to the minimum. This would be the basis to create an own little LPC4370 project based on MCUXpresso.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the big project please navigate to the following file:&amp;nbsp;&amp;nbsp; .\Link2_LED1_Blinky\LPC4330-Xplorer_LedToggle\src\ledtoggle.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to find the short initialization which lets the LED blink. Don't know if all the rest is really used, I just left everything as is, can't remember if it's really required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 17:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Example-code-for-LPC-4370-in-LPC-link2/m-p/1020744#M39881</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-01-30T17:15:43Z</dc:date>
    </item>
  </channel>
</rss>