<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPS55S69 : POWER_CycleCpuAndFlash()</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPS55S69-POWER-CycleCpuAndFlash/m-p/1018286#M39841</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in SDK this API:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief Shut off the Flash and execute the _WFI(), then power up the Flash after wake-up event&lt;BR /&gt; * This MUST BE EXECUTED outside the Flash:&lt;BR /&gt; * either from ROM or from SRAM. The rest could stay in Flash. But, for consistency, it is&lt;BR /&gt; * preferable to have all functions defined in this file implemented in ROM.&lt;BR /&gt; * @param None&lt;BR /&gt; * @return Nothing&lt;BR /&gt; */&lt;BR /&gt;void POWER_CycleCpuAndFlash(void);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But no any information about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can it be more power efficient for Sleep mode than PowerSleep() ?&lt;/P&gt;&lt;P&gt;How I can utilize it in my firmware ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Mar 2020 11:04:05 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2020-03-11T11:04:05Z</dc:date>
    <item>
      <title>LPS55S69 : POWER_CycleCpuAndFlash()</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPS55S69-POWER-CycleCpuAndFlash/m-p/1018286#M39841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in SDK this API:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * @brief Shut off the Flash and execute the _WFI(), then power up the Flash after wake-up event&lt;BR /&gt; * This MUST BE EXECUTED outside the Flash:&lt;BR /&gt; * either from ROM or from SRAM. The rest could stay in Flash. But, for consistency, it is&lt;BR /&gt; * preferable to have all functions defined in this file implemented in ROM.&lt;BR /&gt; * @param None&lt;BR /&gt; * @return Nothing&lt;BR /&gt; */&lt;BR /&gt;void POWER_CycleCpuAndFlash(void);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But no any information about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can it be more power efficient for Sleep mode than PowerSleep() ?&lt;/P&gt;&lt;P&gt;How I can utilize it in my firmware ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 11:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPS55S69-POWER-CycleCpuAndFlash/m-p/1018286#M39841</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-03-11T11:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPS55S69 : POWER_CycleCpuAndFlash()</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPS55S69-POWER-CycleCpuAndFlash/m-p/1018287#M39842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;I have not more information about the function except for the declaration in the fsl_power.h&lt;/P&gt;&lt;P&gt;I will ask the AE team for more inf&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 06:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPS55S69-POWER-CycleCpuAndFlash/m-p/1018287#M39842</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-13T06:50:56Z</dc:date>
    </item>
  </channel>
</rss>