<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 : BoD type of Reset reason</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-BoD-type-of-Reset-reason/m-p/1018193#M39833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In UM chapter 4.6.1 is mentioned that&amp;nbsp;Brown Out Detect (BOD) type of reset can be detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it is not so clear if something should be enabled beforehand.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have plan to keep MCU in Power-down mode and expect if voltage go to low ( but not 0) and return back, reset is happens and via reset reason will be clear that case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be nice to have BoD as wakeup source from Power-Down mode of MCU but it is not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But how to configure MCU for detect BoD type of reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Nov 2019 09:02:03 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2019-11-07T09:02:03Z</dc:date>
    <item>
      <title>LPC55S69 : BoD type of Reset reason</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-BoD-type-of-Reset-reason/m-p/1018193#M39833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In UM chapter 4.6.1 is mentioned that&amp;nbsp;Brown Out Detect (BOD) type of reset can be detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it is not so clear if something should be enabled beforehand.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have plan to keep MCU in Power-down mode and expect if voltage go to low ( but not 0) and return back, reset is happens and via reset reason will be clear that case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be nice to have BoD as wakeup source from Power-Down mode of MCU but it is not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But how to configure MCU for detect BoD type of reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 09:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-BoD-type-of-Reset-reason/m-p/1018193#M39833</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-11-07T09:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : BoD type of Reset reason</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-BoD-type-of-Reset-reason/m-p/1018194#M39834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For topics that are similiar please keep the questions on one thread. If you have follow up questions you may reply in the same posts regarding the same information.&lt;/P&gt;&lt;P&gt;For the answer to this post please refer to the community post.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/517253"&gt;https://community.nxp.com/thread/517253&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 15:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-BoD-type-of-Reset-reason/m-p/1018194#M39834</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-11-08T15:24:50Z</dc:date>
    </item>
  </channel>
</rss>