<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 : Sensitivity of GPIO pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Sensitivity-of-GPIO-pins/m-p/1018132#M39827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;In the datasheet the pin characteristics are described.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95401i508AC4C6F5720152/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The high level input voltage is&amp;nbsp;the voltage level necessary to send to the device for it to read a logic high. The low level input voltage is the voltage level necessary to send to the device for it to read a logic low. Wake up pins can be configured as rising or falling edge.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Nov 2019 04:12:19 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2019-11-12T04:12:19Z</dc:date>
    <item>
      <title>LPC55S69 : Sensitivity of GPIO pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Sensitivity-of-GPIO-pins/m-p/1018131#M39826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have plan to use GPIO pins as part of GINT0/1 group for wakeup MCU from Power-Down mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it is not so clear from DS what kind of sensivity those pins have ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of minimal edge can be detected, is any debounce or glitch filters there and etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have extra info about it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 08:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Sensitivity-of-GPIO-pins/m-p/1018131#M39826</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-11-07T08:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : Sensitivity of GPIO pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Sensitivity-of-GPIO-pins/m-p/1018132#M39827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;In the datasheet the pin characteristics are described.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/95401i508AC4C6F5720152/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The high level input voltage is&amp;nbsp;the voltage level necessary to send to the device for it to read a logic high. The low level input voltage is the voltage level necessary to send to the device for it to read a logic low. Wake up pins can be configured as rising or falling edge.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 04:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Sensitivity-of-GPIO-pins/m-p/1018132#M39827</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-11-12T04:12:19Z</dc:date>
    </item>
  </channel>
</rss>