<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Input Leakage current</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016606#M39786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Peter,&lt;/P&gt;&lt;P&gt;You are right,the pin can be set up as input and output, when the pin is set up in input mode, the output gate is set up in tri-state(High impedance mode), the current is called Ioz. But the Ioz concept is different from the Iil and Iih.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Nov 2019 04:53:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-11-14T04:53:24Z</dc:date>
    <item>
      <title>Input Leakage current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016603#M39783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Data sheet mentions LOW level input current ,high level input current off-state output current and input leakage current.All with a number of footnotes.&lt;/P&gt;&lt;P&gt;Now the HIGH and LOW level input currents are in the nA range , while the input leakage current is in the uA range.&lt;/P&gt;&lt;P&gt;I just wanted to know the sum of leakage currents in the case of using a pin as ADC input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've had several of my colleagues to read this particular section of the data sheet and none of them even gets a remote clue of what this all is supposed to mean.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This data was found in the LPC84x data sheet Ver 1.9 in table 15 on page 54-56 , but it also appeared in the LPC824 datasheet as I recall.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 08:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016603#M39783</guid>
      <dc:creator>p_verheij</dc:creator>
      <dc:date>2019-11-07T08:56:48Z</dc:date>
    </item>
    <item>
      <title>Re: Input Leakage current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016604#M39784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Peter,&lt;/P&gt;&lt;P&gt;I refer to only LPC82x.pdf here.&lt;/P&gt;&lt;P&gt;The IiL is tested with the condition that the pin is an input pin, the input voltage is 0V, the on-chip pull-up resistor is disabled, the input current is 0.5nA generally. Note the spec is valid for general pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94423i6DBB0B39D1A842E4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the following Fig, the Ili(input leakage current) spec is only valid for I2C bus pins(PIO0_10 and PIO0_11 pins), which are open-drain pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/94664iF91A959150FBAF48/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Nov 2019 08:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016604#M39784</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-11-11T08:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: Input Leakage current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016605#M39785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ahhh, i see it now! this 2--4uA leakage current only applies to the I2C lines !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But still remains the issue that every pin id bi-directional, so when you use it as an input , the output is in HI-z state , so I&lt;SPAN style="font-size: 12px;"&gt;oz &lt;SPAN style="font-size: 15px;"&gt; apllies as well as either I&lt;SPAN style="font-size: 12px;"&gt;il&lt;/SPAN&gt; or I&lt;SPAN style="font-size: 12px;"&gt;ih&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 11:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016605#M39785</guid>
      <dc:creator>p_verheij</dc:creator>
      <dc:date>2019-11-12T11:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Input Leakage current</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016606#M39786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Peter,&lt;/P&gt;&lt;P&gt;You are right,the pin can be set up as input and output, when the pin is set up in input mode, the output gate is set up in tri-state(High impedance mode), the current is called Ioz. But the Ioz concept is different from the Iil and Iih.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 04:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Input-Leakage-current/m-p/1016606#M39786</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-11-14T04:53:24Z</dc:date>
    </item>
  </channel>
</rss>