<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Disable crp3 lpc2478</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015813#M39760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Alessandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your requirement, I do not think it is feasible to change the CRP level, after test has completed, restore the original CRP level, because the CRP level is valid only after &amp;nbsp;power off and power on.&lt;/P&gt;&lt;P&gt;Pls refer to part in section &amp;nbsp;8. Code Read Protection (CRP) in UM10237 Reversion 04.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Important: any CRP change becomes effective only after the device has gone&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;through a power cycle.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means that after you change the CRP value, it is not valid until you power off and power on.&lt;/P&gt;&lt;P&gt;The CRP purpose is to block the JTAG port even block bootloader so that invader can not read your code and data from flash or RAM.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jan 2020 03:08:30 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-01-02T03:08:30Z</dc:date>
    <item>
      <title>Disable crp3 lpc2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015812#M39759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone, how can I disable this level of protection and go to other levels also wanting NO_CRP to test and then go back to a level of protection? thanks for the support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2019 07:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015812#M39759</guid>
      <dc:creator>alessandro_dipi</dc:creator>
      <dc:date>2019-12-24T07:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: Disable crp3 lpc2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015813#M39760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Alessandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your requirement, I do not think it is feasible to change the CRP level, after test has completed, restore the original CRP level, because the CRP level is valid only after &amp;nbsp;power off and power on.&lt;/P&gt;&lt;P&gt;Pls refer to part in section &amp;nbsp;8. Code Read Protection (CRP) in UM10237 Reversion 04.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Important: any CRP change becomes effective only after the device has gone&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;through a power cycle.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means that after you change the CRP value, it is not valid until you power off and power on.&lt;/P&gt;&lt;P&gt;The CRP purpose is to block the JTAG port even block bootloader so that invader can not read your code and data from flash or RAM.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2020 03:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015813#M39760</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-01-02T03:08:30Z</dc:date>
    </item>
    <item>
      <title>Re: Disable crp3 lpc2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015814#M39761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Instead I reply saying that I have disabled crp3 from bin file, now if I write the flash with jlink it does not lock even after a cycle of ignitions, so I can rewrite the flash as many times as I want&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2020 17:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015814#M39761</guid>
      <dc:creator>alessandro_dipi</dc:creator>
      <dc:date>2020-01-02T17:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: Disable crp3 lpc2478</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015815#M39762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Alessandro,,&lt;/P&gt;&lt;P&gt;I suppose that you do not write the CRP value to flash which is located at 0x000001FC,pls check it.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2020 09:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Disable-crp3-lpc2478/m-p/1015815#M39762</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-01-03T09:45:30Z</dc:date>
    </item>
  </channel>
</rss>