<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 : wakeup due BoD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-due-BoD/m-p/1014144#M39707</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need BoD type of wakeup when voltage start to drop below some level.&lt;/P&gt;&lt;P&gt;But looks like it is not possible to wakeup MCU from Power-down mode due BoD type of interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can AnalogComparator used in similar way ?&lt;/P&gt;&lt;P&gt;It is not so clear how to initialize it and how some external pins should be used .&lt;/P&gt;&lt;P&gt;Do you have any application note for it or any example usage of it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards !&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Nov 2019 20:11:51 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2019-11-06T20:11:51Z</dc:date>
    <item>
      <title>LPC55S69 : wakeup due BoD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-due-BoD/m-p/1014144#M39707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need BoD type of wakeup when voltage start to drop below some level.&lt;/P&gt;&lt;P&gt;But looks like it is not possible to wakeup MCU from Power-down mode due BoD type of interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can AnalogComparator used in similar way ?&lt;/P&gt;&lt;P&gt;It is not so clear how to initialize it and how some external pins should be used .&lt;/P&gt;&lt;P&gt;Do you have any application note for it or any example usage of it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards !&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2019 20:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-due-BoD/m-p/1014144#M39707</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-11-06T20:11:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : wakeup due BoD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-due-BoD/m-p/1014145#M39708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;If the BOD reset is enabled, the forced BOD reset can wake up the chip from reduced power modes, not including power-down and deep power-down.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/93463iC3B1E4D7DDAC22AA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the analog comparator can be used to wake up the system. An example code is provided in section 14.5.2.4 of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11126"&gt;User Manual&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/93464i955C6C36E98C86E1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pins you are able to use for the analog comparator are the following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/93465iD9B3761F24E4C2CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please specify if you are getting an error when attempting to initialize these pins. This way I can check your code.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 15:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-due-BoD/m-p/1014145#M39708</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-11-08T15:22:33Z</dc:date>
    </item>
  </channel>
</rss>