<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 : minimal PRINCE write chunk</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-minimal-PRINCE-write-chunk/m-p/1013831#M39688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, your assumptions are correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jan 2020 15:40:32 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2020-01-27T15:40:32Z</dc:date>
    <item>
      <title>LPC55S69 : minimal PRINCE write chunk</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-minimal-PRINCE-write-chunk/m-p/1013830#M39687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see SDK example about encryption/description on fly to flash memory by using PRINCE engine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Loading data into the PRINCE - controlled flash area.&lt;BR /&gt; Note, that following conditions must be met (otherwise the error is returned):&lt;BR /&gt; - whole PRINCE subregions (8k block) must be erased at once&lt;BR /&gt; - whole PRINCE subregions (8k block) must be loaded at once (no partial write allowed)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I understand right and 8KB is minimum size for write and erase ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it is not possible to erase 8KB at once and after that write 512 bytes sectors ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 10:33:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-minimal-PRINCE-write-chunk/m-p/1013830#M39687</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-01-15T10:33:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : minimal PRINCE write chunk</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-minimal-PRINCE-write-chunk/m-p/1013831#M39688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, your assumptions are correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 15:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-minimal-PRINCE-write-chunk/m-p/1013831#M39688</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2020-01-27T15:40:32Z</dc:date>
    </item>
  </channel>
</rss>